Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static PhaseRangeOption |
PhaseRangeOption.NEGATIVE_HALF_PI_TO_ONE_HALF_PI
Displays phase between -90 and 270
|
static PhaseRangeOption |
PhaseRangeOption.NEGATIVE_ONE_HALF_PI_TO_HALF_PI
Displays phase between -270 and 90
|
static PhaseRangeOption |
PhaseRangeOption.NEGATIVE_PI_TO_PI
Displays phase between -180 and 180
|
static PhaseRangeOption |
PhaseRangeOption.NEGATIVE_TWO_PI_TO_ZERO
Displays phase between -360 and 0
|
static PhaseRangeOption |
PhaseRangeOption.ZERO_TO_TWO_PI
Displays phase between 0 and 360
|
Modifier and Type | Method and Description |
---|---|
PhaseRangeOption |
Template2D.phaseRangeOption()
Deprecated.
Deprecated in NX10.0.0. Use
CAE.Xyplot.GeneralDisplayStyles#phaseRangeOption instead.
|
PhaseRangeOption |
GeneralDisplayStyles.phaseRangeOption()
Returns the phase range option
License requirements: None. |
static PhaseRangeOption |
PhaseRangeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PhaseRangeOption |
PhaseRangeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PhaseRangeOption[] |
PhaseRangeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Template2D.setPhaseRangeOption(PhaseRangeOption phaseRangeOption)
Deprecated.
Deprecated in NX10.0.0. Use
CAE.Xyplot.GeneralDisplayStyles#setPhaseRangeOption instead.
|
void |
GeneralDisplayStyles.setPhaseRangeOption(PhaseRangeOption phaseRangeOption)
License requirements: nx_ftk ("NX Advanced Graphing") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.