Package | Description |
---|---|
nxopen.cae.xyplot |
Provides classes and interfaces for XY Graphing.
|
Modifier and Type | Field and Description |
---|---|
static GraphStyle |
GraphStyle.BAR
Option to display plot in bar style
|
static GraphStyle |
GraphStyle.LINE
Option to display plot in curve style
|
static GraphStyle |
GraphStyle.PLATE
Option to display plot in plate style
|
static GraphStyle |
GraphStyle.SCATTER
Option to display plot in scatter style
|
static GraphStyle |
GraphStyle.SURFACE
Option to display plot in surface style
|
Modifier and Type | Method and Description |
---|---|
GraphStyle |
DiagramDisplayStyles.getGraphStyle(int styleIndex)
Gets the graph style.
|
GraphStyle |
BaseTemplate.getGraphStyle(int styleIndex)
Deprecated.
Deprecated in NX10.0.0. Use
CAE.Xyplot.DiagramDisplayStyles#getGraphStyle instead.
|
static GraphStyle |
GraphStyle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GraphStyle |
GraphStyle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GraphStyle[] |
GraphStyle.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DiagramDisplayStyles.setGraphStyle(int styleIndex,
GraphStyle graphStyle)
Sets the graph style.
|
void |
BaseTemplate.setGraphStyle(int styleIndex,
GraphStyle graphStyle)
Deprecated.
Deprecated in NX10.0.0. Use
CAE.Xyplot.DiagramDisplayStyles#setGraphStyle instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.