public interface Graph extends TaggedObject
Modifier and Type | Method and Description |
---|---|
MarkerModel |
createMarker(int recordIndex,
int pointIndex)
Creates the display marker on the graph.
|
TaggedObject |
find(String journalIdentifier)
Finds the
NXObject with the given identifier as recorded in a journal. |
MarkerModel[] |
getMarkers()
Gets all markers on the graph.
|
int |
getPointCount(int recordIndex)
Gets the point count of specified record on the graph.
|
int |
recordCount()
Returns the record count of the graph.
|
printTestData, printTestData, tag, tagValue
int recordCount() throws NXException, RemoteException
NXException
RemoteException
int getPointCount(int recordIndex) throws NXException, RemoteException
recordIndex
- Record indexNXException
RemoteException
MarkerModel createMarker(int recordIndex, int pointIndex) throws NXException, RemoteException
CAE.Xyplot.Graph#recordCount
, 0 is inclusive. The point index
is between 0 and CAE.Xyplot.Graph#getPointCount
, 0 is inclusive.
recordIndex
- Record indexpointIndex
- Point indexNXException
RemoteException
MarkerModel[] getMarkers() throws NXException, RemoteException
NXException
RemoteException
TaggedObject find(String journalIdentifier) throws NXException, RemoteException
NXObject
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Journal identifier of the objectNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.