Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
static RSEvent.ResultFileType |
RSEvent.ResultFileType.DYNAMIC_RESPONSE
Result file to contain dynamic response evaluation results, which extension is ".rs2"
|
static RSEvent.ResultFileType |
RSEvent.ResultFileType.FUNCTION_RESPONSE
Result file to contain function response evaluation results, which extenstion is ".afu"
|
static RSEvent.ResultFileType |
RSEvent.ResultFileType.MODAL_RESPONSE
Result file to be used as Restart File, which extension is ".eef" or ".sef"
|
Modifier and Type | Method and Description |
---|---|
static RSEvent.ResultFileType |
RSEvent.ResultFileType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RSEvent.ResultFileType |
RSEvent.ResultFileType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RSEvent.ResultFileType[] |
RSEvent.ResultFileType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
String |
RSEvent.getResultFileName(RSEvent.ResultFileType resultFileType)
Returns result file name of specified type
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.