Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
static InterpolationMethod |
InterpolationMethod.LINEAR_LINEAR |
static InterpolationMethod |
InterpolationMethod.LINEAR_LOG |
static InterpolationMethod |
InterpolationMethod.LOG_LINEAR |
static InterpolationMethod |
InterpolationMethod.LOG_LOG |
Modifier and Type | Method and Description |
---|---|
InterpolationMethod |
RSEventAttributes.interpolationMethod()
Returns the interpolation method. only available when event type is
CAE.ResponseSimulation.RSEvent.Type#FREQUENCY ,
CAE.ResponseSimulation.RSEvent.Type#RANDOM ,
CAE.ResponseSimulation.RSEvent.Type#RESPONSE_SPECTRUM ,
License requirements: nx_response_anlys ("NX Response Analysis") Created in NX5.0.0 |
static InterpolationMethod |
InterpolationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InterpolationMethod |
InterpolationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InterpolationMethod[] |
InterpolationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RSEventAttributes.setInterpolationMethod(InterpolationMethod interpolationMethod)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.