Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static WeldBuilder.PointOnEdgeType |
WeldBuilder.PointOnEdgeType.BY_DISTANCE
Specify the distance between weld points created on an edge
|
static WeldBuilder.PointOnEdgeType |
WeldBuilder.PointOnEdgeType.BY_NUMBER
Specify the number of weld points to be created on an edge
|
static WeldBuilder.PointOnEdgeType |
WeldBuilder.PointOnEdgeType.BY_PATTERN
Specify the distance between weld points as a pattern
|
Modifier and Type | Method and Description |
---|---|
WeldBuilder.PointOnEdgeType |
WeldBuilder.pointOnEdgeOption()
Returns the location of the points on the edge
License requirements: None. |
static WeldBuilder.PointOnEdgeType |
WeldBuilder.PointOnEdgeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldBuilder.PointOnEdgeType |
WeldBuilder.PointOnEdgeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldBuilder.PointOnEdgeType[] |
WeldBuilder.PointOnEdgeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldBuilder.setPointOnEdgeOption(WeldBuilder.PointOnEdgeType pointOnEdgeOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.