Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
ResultAccess |
ResultManager.createResultAccess(int postViewID)
Creates a result access object based on an existing Post View
It is user's responsibility to destroy the result access object once done
using
ResultManager.deleteResultAccess(nxopen.cae.ResultAccess) , in order to free up system resources
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.5.2 |
ResultAccess |
ResultManager.createResultAccess(Result result,
ResultParameters parameters)
Creates a result access object
It is user's responsibility to destroy the result access object once done
using
ResultManager.deleteResultAccess(nxopen.cae.ResultAccess) , in order to free up system resources
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX6.0.2 |
Modifier and Type | Method and Description |
---|---|
void |
ResultManager.deleteResultAccess(ResultAccess result)
Delete a
ResultAccess object. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.