Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.GroupContainer |
Result.GroupContainer.CONNECTOR |
static Result.GroupContainer |
Result.GroupContainer.ONE_DIMENSIONAL |
static Result.GroupContainer |
Result.GroupContainer.OTHER |
static Result.GroupContainer |
Result.GroupContainer.THREE_DIMENSIONAL |
static Result.GroupContainer |
Result.GroupContainer.TWO_DIMENSIONAL |
static Result.GroupContainer |
Result.GroupContainer.ZERO_DIMENSIONAL |
Modifier and Type | Method and Description |
---|---|
static Result.GroupContainer |
Result.GroupContainer.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.GroupContainer |
Result.GroupContainer.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.GroupContainer[] |
Result.GroupContainer.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
int[] |
Result.askNumElementsOfGroup(Result.GroupContainer type,
int groupIndex)
Returns an array of elements indices for a given group
Group index range from 0 to N-1 (number of groups)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int |
Result.askNumGroupsInContainer(Result.GroupContainer type)
Returns the number of groups available in the model of type
Result.GroupContainer
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX6.0.2 |
void |
Post.postviewApplyGroupContainerVisibility(int postviewId,
Result.GroupContainer[] container,
boolean visibility)
Set the visibility of an element group container(s) in the input postview id with immediate effect.
|
void |
Post.postviewApplyGroupContainerVisibility(int postviewId,
Result.GroupContainer container,
boolean visibility)
Set the visibility of an element group container in the input postview id with immediate effect.
|
void |
Post.postviewApplyGroupVisibility(int postviewId,
Result.GroupContainer[] container,
int[] group,
boolean visibility)
Set the visibility of an element group(s) (index) within a container (1D, 2D, Connector etc) in
the input postview id with immediate effect.
|
void |
Post.postviewApplyGroupVisibility(int postviewId,
Result.GroupContainer container,
int group,
boolean visibility)
Set the visibility of an element group (index) within a container (1D, 2D, Connector etc) in
the input postview id with immediate effect.
|
void |
Post.postviewSetGroupContainerVisibility(int postviewId,
Result.GroupContainer container,
boolean visibility)
Set the visibility of an element group container in the input postview id.
|
void |
Post.postviewSetGroupVisibility(int postviewId,
Result.GroupContainer container,
int group,
boolean visibility)
Set the visibility of an element group (index) within a container (1D, 2D, Connector etc) in
the input postview id.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.