Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.AVERAGE |
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.INTEGRAL |
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.MAXIMUM |
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.MINIMUM |
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.SUM |
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.WEIGHTED_AVERAGE |
Modifier and Type | Method and Description |
---|---|
PostGraphBuilder.GeometryValue |
PostGraphBuilder.geometryCombinationValue()
Returns the geometry value option in case of edge, face or body selection
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.GeometryValue |
PostGraphBuilder.GeometryValue.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.GeometryValue[] |
PostGraphBuilder.GeometryValue.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphBuilder.setGeometryCombinationValue(PostGraphBuilder.GeometryValue geometryValue)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.