Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphBuilder.EdgeIntegralOption |
PostGraphBuilder.EdgeIntegralOption.AREA |
static PostGraphBuilder.EdgeIntegralOption |
PostGraphBuilder.EdgeIntegralOption.LENGTH |
Modifier and Type | Method and Description |
---|---|
PostGraphBuilder.EdgeIntegralOption |
PostGraphBuilder.edgeIntegralOptionValue()
Returns the weighted average or integral option on selecting Edge
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static PostGraphBuilder.EdgeIntegralOption |
PostGraphBuilder.EdgeIntegralOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.EdgeIntegralOption |
PostGraphBuilder.EdgeIntegralOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.EdgeIntegralOption[] |
PostGraphBuilder.EdgeIntegralOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphBuilder.setEdgeIntegralOptionValue(PostGraphBuilder.EdgeIntegralOption edgeIntegralOption)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.