Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphAlongPathBuilder.Xaxis |
PostGraphAlongPathBuilder.Xaxis.COORDINATE_VALUE_OF_COORDINATE_SYSTEM_AXIS |
static PostGraphAlongPathBuilder.Xaxis |
PostGraphAlongPathBuilder.Xaxis.IDS |
static PostGraphAlongPathBuilder.Xaxis |
PostGraphAlongPathBuilder.Xaxis.LENGTH_ALONG_DIRECTION |
static PostGraphAlongPathBuilder.Xaxis |
PostGraphAlongPathBuilder.Xaxis.PATH_LENGTH |
Modifier and Type | Method and Description |
---|---|
static PostGraphAlongPathBuilder.Xaxis |
PostGraphAlongPathBuilder.Xaxis.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphAlongPathBuilder.Xaxis |
PostGraphAlongPathBuilder.Xaxis.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphAlongPathBuilder.Xaxis[] |
PostGraphAlongPathBuilder.Xaxis.values()
Returns an array that contains the values for this enum.
|
PostGraphAlongPathBuilder.Xaxis |
PostGraphAlongPathBuilder.xaxisOption()
Returns the option for defining the x axis of the graph.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphAlongPathBuilder.setXaxisOption(PostGraphAlongPathBuilder.Xaxis xaxis)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.