Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphAlongPathBuilder.CoordinateSysAxis |
PostGraphAlongPathBuilder.CoordinateSysAxis.FIRST_AXIS |
static PostGraphAlongPathBuilder.CoordinateSysAxis |
PostGraphAlongPathBuilder.CoordinateSysAxis.SECOND_AXIS |
static PostGraphAlongPathBuilder.CoordinateSysAxis |
PostGraphAlongPathBuilder.CoordinateSysAxis.THIRD_AXIS |
Modifier and Type | Method and Description |
---|---|
PostGraphAlongPathBuilder.CoordinateSysAxis |
PostGraphAlongPathBuilder.csysAxis()
Returns the option to define the coordinate system axis to be used when x axis defined by
PostGraphAlongPathBuilder.Xaxis.COORDINATE_VALUE_OF_COORDINATE_SYSTEM_AXIS
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX9.0.0 |
static PostGraphAlongPathBuilder.CoordinateSysAxis |
PostGraphAlongPathBuilder.CoordinateSysAxis.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphAlongPathBuilder.CoordinateSysAxis |
PostGraphAlongPathBuilder.CoordinateSysAxis.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphAlongPathBuilder.CoordinateSysAxis[] |
PostGraphAlongPathBuilder.CoordinateSysAxis.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphAlongPathBuilder.setCsysAxis(PostGraphAlongPathBuilder.CoordinateSysAxis axis)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.