Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.AVERAGE |
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.DIFFERENCE |
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.INTEGRAL |
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.MAXIMUM |
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.MINIMUM |
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.SUM |
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.WEIGHTED_AVERAGE |
Modifier and Type | Method and Description |
---|---|
PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.combineValueFromEntitiesOption()
Returns the set combine across entities option type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphAcrossIterationsBuilder.CombinationMethod |
PostGraphAcrossIterationsBuilder.CombinationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphAcrossIterationsBuilder.CombinationMethod[] |
PostGraphAcrossIterationsBuilder.CombinationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphAcrossIterationsBuilder.setCombineValueFromEntitiesOption(PostGraphAcrossIterationsBuilder.CombinationMethod combineOption)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.