Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
Post.AnimationStyle |
Post.Animation.animationStyle |
static Post.AnimationStyle |
Post.AnimationStyle.LINEAR |
static Post.AnimationStyle |
Post.AnimationStyle.MODAL |
Modifier and Type | Method and Description |
---|---|
static Post.AnimationStyle |
Post.AnimationStyle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.AnimationStyle |
Post.AnimationStyle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.AnimationStyle[] |
Post.AnimationStyle.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
Animation(Post.AnimationType animationTypeInitial,
Post.AnimationStyle animationStyleInitial,
int numberOfFramesInitial,
int startLoadcaseInitial,
int startIterationInitial,
int endLoadcaseInitial,
int endIterationInitial,
int iterationIncrementInitial,
boolean fullCycleInitial,
int delayInitial,
Post.AnimationStreamline animationStreamlineInitial,
Post.AnimationIterationTypes iterationTypeInitial)
Constructor for the Animation object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.