Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
Post.AnimationStreamline |
Post.Animation.animationStreamline |
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewAnimationControlStreamline(int postviewId,
Post.AnimationStreamline control)
Control streamline animation for the input postview id
The input postview id is what was returned from CreatePostview or CreatePostviewForResult.
|
Constructor and Description |
---|
Animation(Post.AnimationType animationTypeInitial,
Post.AnimationStyle animationStyleInitial,
int numberOfFramesInitial,
int startLoadcaseInitial,
int startIterationInitial,
int endLoadcaseInitial,
int endIterationInitial,
int iterationIncrementInitial,
boolean fullCycleInitial,
int delayInitial,
Post.AnimationStreamline animationStreamlineInitial,
Post.AnimationIterationTypes iterationTypeInitial)
Constructor for the Animation object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.