Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.AnimationControl |
Post.AnimationControl.BACK |
static Post.AnimationControl |
Post.AnimationControl.DELAY |
static Post.AnimationControl |
Post.AnimationControl.FULL_CYCLE |
static Post.AnimationControl |
Post.AnimationControl.NEXT |
static Post.AnimationControl |
Post.AnimationControl.PAUSE |
static Post.AnimationControl |
Post.AnimationControl.PLAY |
static Post.AnimationControl |
Post.AnimationControl.SET_FRAME |
static Post.AnimationControl |
Post.AnimationControl.STOP |
static Post.AnimationControl |
Post.AnimationControl.STREAMLINE |
Modifier and Type | Method and Description |
---|---|
static Post.AnimationControl |
Post.AnimationControl.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.AnimationControl |
Post.AnimationControl.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.AnimationControl[] |
Post.AnimationControl.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewAnimationControl(int postviewId,
Post.AnimationControl control,
int frame,
boolean fullCycle,
int delay)
Control animation for the input postview id
The input postview id is what was returned from CreatePostview or CreatePostviewForResult
This interface works only in interactive mode.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.