Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
MeshManualSweepBetweenListItemSelection |
Mesh3dHexBuilder.createNewListItem(CAEEdge tMasterEdge,
CAEEdge tTargetEdge,
boolean fFlipDirection)
The list item
License requirements: nx_masterfem ("Finite Element Modeling") . |
MeshManualSweepBetweenListItemSelection |
MeshManualSweepBetweenListItemSelectionList.findItem(int index)
Returns the object at the input index.
|
MeshManualSweepBetweenListItemSelection[] |
MeshManualSweepBetweenListItemSelectionList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
MeshManualSweepBetweenListItemSelectionList.append(MeshManualSweepBetweenListItemSelection object)
Appends an object to the list
License requirements: None. |
void |
MeshManualSweepBetweenListItemSelectionList.append(MeshManualSweepBetweenListItemSelection[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
MeshManualSweepBetweenListItemSelectionList.erase(MeshManualSweepBetweenListItemSelection obj)
Erases the object from the list, but does not delete the object.
|
void |
MeshManualSweepBetweenListItemSelectionList.erase(MeshManualSweepBetweenListItemSelection obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
MeshManualSweepBetweenListItemSelectionList.findIndex(MeshManualSweepBetweenListItemSelection obj)
Finds the index where the input object appears.
|
void |
MeshManualSweepBetweenListItemSelectionList.insert(int location,
MeshManualSweepBetweenListItemSelection object)
Inserts an object at the specified location
License requirements: None. |
void |
MeshManualSweepBetweenListItemSelectionList.setContents(MeshManualSweepBetweenListItemSelection[] objects)
Sets the contents of the entire list.
|
void |
MeshManualSweepBetweenListItemSelectionList.swap(MeshManualSweepBetweenListItemSelection object1,
MeshManualSweepBetweenListItemSelection object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.