Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ElementExtrudeBuilder.MethodType |
ElementExtrudeBuilder.MethodType.ELEM_NORMAL
along element normal
|
static ElementExtrudeBuilder.MethodType |
ElementExtrudeBuilder.MethodType.PATH
along path
|
static ElementExtrudeBuilder.MethodType |
ElementExtrudeBuilder.MethodType.PROJ_SURFACE
project to surface
|
static ElementExtrudeBuilder.MethodType |
ElementExtrudeBuilder.MethodType.VECTOR
along vector
|
Modifier and Type | Method and Description |
---|---|
ElementExtrudeBuilder.MethodType |
ElementExtrudeBuilder.methodOption()
Returns the method option
License requirements: None. |
static ElementExtrudeBuilder.MethodType |
ElementExtrudeBuilder.MethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementExtrudeBuilder.MethodType |
ElementExtrudeBuilder.MethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementExtrudeBuilder.MethodType[] |
ElementExtrudeBuilder.MethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ElementExtrudeBuilder.setMethodOption(ElementExtrudeBuilder.MethodType methodOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.