Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static EdgeSticherBuilder.StitchOptions |
EdgeSticherBuilder.StitchOptions.BOTH |
static EdgeSticherBuilder.StitchOptions |
EdgeSticherBuilder.StitchOptions.EDGE_TO_EDGES |
static EdgeSticherBuilder.StitchOptions |
EdgeSticherBuilder.StitchOptions.EDGE_TO_FACES |
Modifier and Type | Method and Description |
---|---|
EdgeSticherBuilder.StitchOptions |
EdgeSticherBuilder.stitchOption()
Returns the operand type for auto-stitch edge
License requirements: None. |
static EdgeSticherBuilder.StitchOptions |
EdgeSticherBuilder.StitchOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeSticherBuilder.StitchOptions |
EdgeSticherBuilder.StitchOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeSticherBuilder.StitchOptions[] |
EdgeSticherBuilder.StitchOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeSticherBuilder.setStitchOption(EdgeSticherBuilder.StitchOptions stitchOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.