Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CfdContactPreventionConstraintBuilder.Sizing |
CfdContactPreventionConstraintBuilder.Sizing.ABSOLUTE |
static CfdContactPreventionConstraintBuilder.Sizing |
CfdContactPreventionConstraintBuilder.Sizing.RELATIVE_COARSENING |
static CfdContactPreventionConstraintBuilder.Sizing |
CfdContactPreventionConstraintBuilder.Sizing.RELATIVE_REFINEMENT |
Modifier and Type | Method and Description |
---|---|
CfdContactPreventionConstraintBuilder.Sizing |
CfdContactPreventionConstraintBuilder.sizingOption()
Returns the sizing option
License requirements: None. |
static CfdContactPreventionConstraintBuilder.Sizing |
CfdContactPreventionConstraintBuilder.Sizing.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CfdContactPreventionConstraintBuilder.Sizing |
CfdContactPreventionConstraintBuilder.Sizing.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CfdContactPreventionConstraintBuilder.Sizing[] |
CfdContactPreventionConstraintBuilder.Sizing.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CfdContactPreventionConstraintBuilder.setSizingOption(CfdContactPreventionConstraintBuilder.Sizing sizingOption)
License requirements: nx_adv_fluid_mod ("NX Advanced Fluid Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.