Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static AssignNodalCSBuilder.GeometryOption |
AssignNodalCSBuilder.GeometryOption.BOUNDARY_NODES_ONLY
boundary nodes only
|
static AssignNodalCSBuilder.GeometryOption |
AssignNodalCSBuilder.GeometryOption.INTERIOR_NODES_ONLY
interior nodes only
|
static AssignNodalCSBuilder.GeometryOption |
AssignNodalCSBuilder.GeometryOption.INTERIORAND_BOUNDARY_NODES
interior and boundary
|
Modifier and Type | Method and Description |
---|---|
AssignNodalCSBuilder.GeometryOption |
AssignNodalCSBuilder.boundaryOptions()
Returns the boundary options
License requirements: None. |
static AssignNodalCSBuilder.GeometryOption |
AssignNodalCSBuilder.GeometryOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssignNodalCSBuilder.GeometryOption |
AssignNodalCSBuilder.GeometryOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssignNodalCSBuilder.GeometryOption[] |
AssignNodalCSBuilder.GeometryOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssignNodalCSBuilder.setBoundaryOptions(AssignNodalCSBuilder.GeometryOption boundaryOptions)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.