public static class TransientResultsReductionBuilder.EvaluationError extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABORT |
static int |
_SKIP |
static int |
_ZERO_FILL |
static TransientResultsReductionBuilder.EvaluationError |
ABORT |
static TransientResultsReductionBuilder.EvaluationError |
SKIP |
static TransientResultsReductionBuilder.EvaluationError |
ZERO_FILL |
Modifier and Type | Method and Description |
---|---|
static TransientResultsReductionBuilder.EvaluationError |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TransientResultsReductionBuilder.EvaluationError |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TransientResultsReductionBuilder.EvaluationError[] |
values()
Returns an array that contains the values for this enum.
|
public static final TransientResultsReductionBuilder.EvaluationError SKIP
public static final TransientResultsReductionBuilder.EvaluationError ZERO_FILL
public static final TransientResultsReductionBuilder.EvaluationError ABORT
public static final int _SKIP
public static final int _ZERO_FILL
public static final int _ABORT
public static TransientResultsReductionBuilder.EvaluationError valueOf(int value)
public static TransientResultsReductionBuilder.EvaluationError valueOf(String name)
public static TransientResultsReductionBuilder.EvaluationError[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.