public interface ResultMeasureCollection extends TaggedObjectCollection
ResultMeasure
SimSimulation
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
ResultMeasureModelSubset |
createModelSubset(ResultMeasure.SubsetSelection eSubset)
Create a model subset for result measure
License requirements: nx_masterfem ("Finite Element Modeling") . |
ResultMeasure |
createResultMeasure(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp,
String expName)
Deprecated.
Deprecated in NX10.0.0. Use
createResultMeasureNew(nxopen.cae.ResultMeasureResultOptions, nxopen.cae.ResultMeasureModelSubset, java.lang.String) instead.
|
ResultMeasure |
createResultMeasureNew(ResultMeasureResultOptions pResOpt,
ResultMeasureModelSubset pSubset,
String expName)
Create a ResultMeasure
License requirements: nx_masterfem ("Finite Element Modeling") . |
ResultMeasureResultOptions |
createResultOptions(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :createResultMeasureNew(nxopen.cae.ResultMeasureResultOptions, nxopen.cae.ResultMeasureModelSubset, java.lang.String) instead.
|
ResultMeasureResultOptions |
createResultOptionsNew(SimSolution tSol,
SimResultReference tResultReference,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Create a result options for result measure
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
deleteMeasures(ResultMeasure[] objects)
Delete list of result measures
License requirements: nx_masterfem ("Finite Element Modeling") . |
ResultMeasure |
find(String journalIdentifier)
Finds the
ResultMeasure with the given identifier as recorded in a journal. |
void |
updateMeasures(ResultMeasure[] objects)
Update list of result measures.
|
_find_next, iterator
ResultMeasure createResultMeasure(SimSolution tSol, int iStepIndex, int iIterIndex, Result.Type pType, Result.Component eComp, String expName) throws NXException, RemoteException
createResultMeasureNew(nxopen.cae.ResultMeasureResultOptions, nxopen.cae.ResultMeasureModelSubset, java.lang.String)
instead.
tSol
- iStepIndex
- iIterIndex
- pType
- eComp
- expName
- NXException
RemoteException
ResultMeasure find(String journalIdentifier) throws NXException, RemoteException
ResultMeasure
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Identifier of the ResultMeasure you wantNXException
RemoteException
void updateMeasures(ResultMeasure[] objects) throws NXException, RemoteException
objects
- The objects to be updatedNXException
RemoteException
void deleteMeasures(ResultMeasure[] objects) throws NXException, RemoteException
objects
- The objects to be updatedNXException
RemoteException
ResultMeasureResultOptions createResultOptions(SimSolution tSol, int iStepIndex, int iIterIndex, Result.Type pType, Result.Component eComp) throws NXException, RemoteException
SimResultReference
:createResultMeasureNew(nxopen.cae.ResultMeasureResultOptions, nxopen.cae.ResultMeasureModelSubset, java.lang.String)
instead.
tSol
- iStepIndex
- iIterIndex
- pType
- eComp
- NXException
RemoteException
ResultMeasureResultOptions createResultOptionsNew(SimSolution tSol, SimResultReference tResultReference, int iStepIndex, int iIterIndex, Result.Type pType, Result.Component eComp) throws NXException, RemoteException
tSol
- tResultReference
- iStepIndex
- iIterIndex
- pType
- eComp
- NXException
RemoteException
ResultMeasureModelSubset createModelSubset(ResultMeasure.SubsetSelection eSubset) throws NXException, RemoteException
eSubset
- NXException
RemoteException
ResultMeasure createResultMeasureNew(ResultMeasureResultOptions pResOpt, ResultMeasureModelSubset pSubset, String expName) throws NXException, RemoteException
pResOpt
- pSubset
- The model subset, can be nullexpName
- The new expression name for the result measure NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.