public static class AutomaticMorphBuilder.OrphanNodeMovementType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BASED_ON_NBR_MOVEMENT
Based on adjacent nodes movement.
|
static int |
_STATIONARY
Stationary in topologically modified region.
|
static AutomaticMorphBuilder.OrphanNodeMovementType |
BASED_ON_NBR_MOVEMENT
Based on adjacent nodes movement.
|
static AutomaticMorphBuilder.OrphanNodeMovementType |
STATIONARY
Stationary in topologically modified region.
|
Modifier and Type | Method and Description |
---|---|
static AutomaticMorphBuilder.OrphanNodeMovementType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutomaticMorphBuilder.OrphanNodeMovementType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutomaticMorphBuilder.OrphanNodeMovementType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AutomaticMorphBuilder.OrphanNodeMovementType BASED_ON_NBR_MOVEMENT
public static final AutomaticMorphBuilder.OrphanNodeMovementType STATIONARY
public static final int _BASED_ON_NBR_MOVEMENT
public static final int _STATIONARY
public static AutomaticMorphBuilder.OrphanNodeMovementType valueOf(int value)
public static AutomaticMorphBuilder.OrphanNodeMovementType valueOf(String name)
public static AutomaticMorphBuilder.OrphanNodeMovementType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.