public interface AfuData extends TransientObject
Modifier and Type | Interface and Description |
---|---|
static class |
AfuData.AbscissaAndOrdinateAxisDefinitionData
This class holds the data returned from
getAbscissaAndOrdinateAxisDefinition() |
static class |
AfuData.AbscissaType
Defines abscissa data type for AFU data record
|
static class |
AfuData.AxisDefinitionData
This class holds the data returned from
getAxisDefinition() |
static class |
AfuData.ComplexData
This class holds the data returned from
getComplexData() |
static class |
AfuData.EvenData
This class holds the data returned from
getEvenData() |
static class |
AfuData.IdInformationData
This class holds the data returned from
getIdInformation() |
static class |
AfuData.OrdinateType
Defines ordinate data type for AFU data record
|
static class |
AfuData.RealData
This class holds the data returned from
getRealData() |
Modifier and Type | Method and Description |
---|---|
AfuAbscissaHeaderInfo |
afuAbscissaHeaderInfo()
Returns the abscissa header information data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
AfuHeaderId |
afuHeaderId()
Returns the AFU Header Id data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
AfuOrdinateHeaderInfo |
afuOrdinateHeaderInfo()
Returns the ordinate header information data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
AfuZHeaderInfo |
afuZHeaderInfo()
Returns the Z axis header information data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
String |
fileName()
Returns the name of AFU file
License requirements: nx_ftk ("NX Advanced Graphing") . |
XyFunctionDataType |
functionDataType()
Returns the data type of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
AfuData.AbscissaAndOrdinateAxisDefinitionData |
getAbscissaAndOrdinateAxisDefinition()
Get the Abscissa and Ordinate Axis definitions of an AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
AfuData.AxisDefinitionData |
getAxisDefinition()
Deprecated.
Deprecated in NX9.0.0. Use
getAbscissaAndOrdinateAxisDefinition() with Denominator.
|
AfuData.ComplexData |
getComplexData()
Get the XY data of an AFU Data Record when the ordinate type is Complex
License requirements: nx_ftk ("NX Advanced Graphing") . |
AfuData.EvenData |
getEvenData()
Get the Abscissa Information for an AFU Data Record when the abscissa type is even
License requirements: nx_ftk ("NX Advanced Graphing") . |
AfuData.IdInformationData |
getIdInformation()
Deprecated.
Deprecated in NX10.0.0. Use
afuHeaderId() instead.
|
AfuData.RealData |
getRealData()
Get the XY Data of an AFU Data Record when the ordinate type is real
License requirements: nx_ftk ("NX Advanced Graphing") . |
String |
recordName()
Returns the name of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setAbscissaAndOrdinateAxisDefinition(XyFunctionUnit xUnit,
AfuData.OrdinateType ordinateType,
XyFunctionUnit yUnit,
XyFunctionUnit yDenominatorUnit)
Set the Abscissa and Ordinate Axis definitions of an AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setAfuAbscissaHeaderInfo(AfuAbscissaHeaderInfo abscissaHeaderInfo)
Sets the abscissa header information data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setAfuHeaderId(AfuHeaderId afuHeaderId)
Sets the AFU Header Id data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setAfuOrdinateHeaderInfo(AfuOrdinateHeaderInfo ordinateHeaderInfo)
Sets the ordinate header information data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setAfuZHeaderInfo(AfuZHeaderInfo zHeaderInfoP)
Sets the Z axis header information data of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setAxisDefinition(AfuData.AbscissaType abscissaType,
XyFunctionUnit xUnit,
AfuData.OrdinateType oridinateType,
XyFunctionUnit yUnit)
Deprecated.
Deprecated in NX9.0.0. Use
setAbscissaAndOrdinateAxisDefinition(nxopen.cae.XyFunctionUnit, nxopen.cae.AfuData.OrdinateType, nxopen.cae.XyFunctionUnit, nxopen.cae.XyFunctionUnit) with Denominator.
|
void |
setComplexData(double[] xValues,
double[] yValues,
double[] zValues)
Set the XY Data of an AFU record when the ordinate type is Complex
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setComplexData(double xMinimum,
double xIncrement,
double[] yValues,
double[] zValues)
Set the XY Data of an AFU record when the ordinate type is Complex
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setEvenData(double xMinimum,
double xIncrement,
int numberOfPoints)
Deprecated.
Deprecated in NX9.0.0. Use
setRealData(double[], double[]) or setComplexData(double[], double[], double[]) that takes minimum abscissa value and increment instead.
|
void |
setFileName(String afuFileName)
Sets the name of AFU file
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setFunctionDataType(XyFunctionDataType functionDataType)
Sets the data type of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setIdInformation(String reference,
int referenceId,
String response,
int responseId)
Deprecated.
Deprecated in NX10.0.0. Use
setAfuHeaderId(nxopen.cae.AfuHeaderId) instead.
|
void |
setRealData(double[] xValues,
double[] yValues)
Set the XY Data of an AFU Data Record when the ordinate type is real
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setRealData(double xMinimum,
double xIncrement,
double[] yValues)
Set the XY Data of an AFU Data Record when the ordinate type is real and the absicssa type is even
License requirements: nx_ftk ("NX Advanced Graphing") . |
void |
setRecordName(String afuRecordName)
Sets the name of the AFU Data Record
License requirements: nx_ftk ("NX Advanced Graphing") . |
_value, dispose, printTestData, printTestData
void setFileName(String afuFileName) throws NXException, RemoteException
afuFileName
- The full name of the AFU fileNXException
RemoteException
String fileName() throws NXException, RemoteException
NXException
RemoteException
void setRecordName(String afuRecordName) throws NXException, RemoteException
afuRecordName
- The name of AFU Data RecordNXException
RemoteException
String recordName() throws NXException, RemoteException
NXException
RemoteException
void setIdInformation(String reference, int referenceId, String response, int responseId) throws NXException, RemoteException
setAfuHeaderId(nxopen.cae.AfuHeaderId)
instead.
reference
- String to define reference direction sense.
Up to 4 characters are allowed and
the redundant characters will be ignored.
( X, Y, Z, RX, RY, and RZ have specific
meaning but the character set can be
anything including a "+" or "-" as the
last character. examples: ABC+ RSTU )
referenceId
- ID of reference element or noderesponse
- String to define response direction sense.
Up to 4 characters are allowed and the redundant
characters will be ignored.
( X, Y, Z, RX, RY, and RZ have specific
meaning but the character set can be
anything including a "+" or "-" as the
last character. examples: ABC+ RSTU )
responseId
- ID of response element or node
NXException
RemoteException
AfuData.IdInformationData getIdInformation() throws NXException, RemoteException
afuHeaderId()
instead.
NXException
RemoteException
void setAxisDefinition(AfuData.AbscissaType abscissaType, XyFunctionUnit xUnit, AfuData.OrdinateType oridinateType, XyFunctionUnit yUnit) throws NXException, RemoteException
setAbscissaAndOrdinateAxisDefinition(nxopen.cae.XyFunctionUnit, nxopen.cae.AfuData.OrdinateType, nxopen.cae.XyFunctionUnit, nxopen.cae.XyFunctionUnit)
with Denominator.
abscissaType
- Abscissa specific data typexUnit
- Unit Code of abscissa dataoridinateType
- Ordinate specific data typeyUnit
- Unit Code of ordinate data
NXException
RemoteException
void setAbscissaAndOrdinateAxisDefinition(XyFunctionUnit xUnit, AfuData.OrdinateType ordinateType, XyFunctionUnit yUnit, XyFunctionUnit yDenominatorUnit) throws NXException, RemoteException
xUnit
- Unit Code of abscissa dataordinateType
- Ordinate data typeyUnit
- Unit Code of ordinate datayDenominatorUnit
- Unit Code of ordinate dataNXException
RemoteException
AfuData.AxisDefinitionData getAxisDefinition() throws NXException, RemoteException
getAbscissaAndOrdinateAxisDefinition()
with Denominator.
NXException
RemoteException
AfuData.AbscissaAndOrdinateAxisDefinitionData getAbscissaAndOrdinateAxisDefinition() throws NXException, RemoteException
NXException
RemoteException
void setEvenData(double xMinimum, double xIncrement, int numberOfPoints) throws NXException, RemoteException
setRealData(double[], double[])
or setComplexData(double[], double[], double[])
that takes minimum abscissa value and increment instead.
xMinimum
- Minimum abscissa data valuexIncrement
- Abscissa incrementnumberOfPoints
- Number of abscissa elements
NXException
RemoteException
AfuData.EvenData getEvenData() throws NXException, RemoteException
NXException
RemoteException
void setRealData(double[] xValues, double[] yValues) throws NXException, RemoteException
xValues
- Abscissa element data valuesyValues
- Ordinate element data valuesNXException
RemoteException
void setRealData(double xMinimum, double xIncrement, double[] yValues) throws NXException, RemoteException
xMinimum
- Minimum abscissa data valuexIncrement
- Abscissa incrementyValues
- Ordinate element data valuesNXException
RemoteException
AfuData.RealData getRealData() throws NXException, RemoteException
NXException
RemoteException
void setComplexData(double[] xValues, double[] yValues, double[] zValues) throws NXException, RemoteException
xValues
- Abscissa element data valuesyValues
- Ordinate element data values for real part or magnitude partzValues
- Ordinate element data values for imaginary part or phase partNXException
RemoteException
void setComplexData(double xMinimum, double xIncrement, double[] yValues, double[] zValues) throws NXException, RemoteException
xMinimum
- Minimum abscissa data valuexIncrement
- Abscissa incrementyValues
- Ordinate element data values for real part or magnitude partzValues
- Ordinate element data values for imaginary part or phase partNXException
RemoteException
AfuData.ComplexData getComplexData() throws NXException, RemoteException
NXException
RemoteException
void setFunctionDataType(XyFunctionDataType functionDataType) throws NXException, RemoteException
functionDataType
- The data type of a function in AFUNXException
RemoteException
XyFunctionDataType functionDataType() throws NXException, RemoteException
NXException
RemoteException
void setAfuHeaderId(AfuHeaderId afuHeaderId) throws NXException, RemoteException
afuHeaderId
- The AFU Header Id dataNXException
RemoteException
AfuHeaderId afuHeaderId() throws NXException, RemoteException
NXException
RemoteException
void setAfuAbscissaHeaderInfo(AfuAbscissaHeaderInfo abscissaHeaderInfo) throws NXException, RemoteException
abscissaHeaderInfo
- Abscissa header information data CAE.AfuAbscissaHeaderInfo
to be setNXException
RemoteException
AfuAbscissaHeaderInfo afuAbscissaHeaderInfo() throws NXException, RemoteException
CAE.AfuAbscissaHeaderInfo
to be getNXException
RemoteException
void setAfuOrdinateHeaderInfo(AfuOrdinateHeaderInfo ordinateHeaderInfo) throws NXException, RemoteException
ordinateHeaderInfo
- Ordindate header information data CAE.AfuOrdinateHeaderInfo
to be setNXException
RemoteException
AfuOrdinateHeaderInfo afuOrdinateHeaderInfo() throws NXException, RemoteException
CAE.AfuOrdinateHeaderInfo
to be getNXException
RemoteException
void setAfuZHeaderInfo(AfuZHeaderInfo zHeaderInfoP) throws NXException, RemoteException
zHeaderInfoP
- Z axis header information data CAE.AfuZHeaderInfo
to be setNXException
RemoteException
AfuZHeaderInfo afuZHeaderInfo() throws NXException, RemoteException
CAE.AfuZHeaderInfo
to be getNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.