Package | Description |
---|---|
nxopen.blockstyler |
Provides classes and interfaces for the Block Styler.
|
Modifier and Type | Field and Description |
---|---|
static BlockDialog.DialogMode |
BlockDialog.DialogMode.CREATE
When the user presses Ok or Apply on the
dialog, the user's inputs are saved in dialog memory and the next time that the dialog
is shown in Create mode, the dialog is initialized using the user's previous
inputs.
|
static BlockDialog.DialogMode |
BlockDialog.DialogMode.EDIT
The Apply button is not shown.
|
Modifier and Type | Method and Description |
---|---|
static BlockDialog.DialogMode |
BlockDialog.DialogMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlockDialog.DialogMode |
BlockDialog.DialogMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlockDialog.DialogMode[] |
BlockDialog.DialogMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
Selection.Response |
BlockDialog.show(BlockDialog.DialogMode dialogMode)
Shows the dialog in
BlockStyler.BlockDialog.DialogMode#CREATE OR BlockStyler.BlockDialog.DialogMode#EDIT mode based on input
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.