Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ClearanceSet.JobStatus |
ClearanceSet.JobStatus.ABORTED_BY_USER |
static ClearanceSet.JobStatus |
ClearanceSet.JobStatus.ABORTED_ON_ERROR |
ClearanceSet.JobStatus |
ClearanceSet.Summary.jobStatus
Indicates if the analysis was
aborted.
|
static ClearanceSet.JobStatus |
ClearanceSet.JobStatus.NOT_ABORTED |
Modifier and Type | Method and Description |
---|---|
static ClearanceSet.JobStatus |
ClearanceSet.JobStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClearanceSet.JobStatus |
ClearanceSet.JobStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClearanceSet.JobStatus[] |
ClearanceSet.JobStatus.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
Summary(int startTimeInitial,
int endTimeInitial,
int runTimeInitial,
int versionInitial,
ClearanceAnalysisBuilder.CalculationMethodType analysisModeInitial,
int numCollectionsInitial,
int numCollection1Initial,
int numCollection2Initial,
int numPairsInitial,
int numExcludedPairsInitial,
int numChangedPairsInitial,
int numChangedObjsInitial,
int numCheckedPairsInitial,
int numNewHardInitial,
int numNewSoftInitial,
int numNewTouchingInitial,
int numNewContainmentInitial,
int numNewAllInterfInitial,
int numHardInitial,
int numSoftInitial,
int numTouchingInitial,
int numContainmentInitial,
int numAllInterfInitial,
ClearanceSet.JobStatus jobStatusInitial,
int numZonesInitial)
Constructor for the Summary object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.