Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BalloonNote
Represents a Balloon Note
To create or edit an instance of this class, use BalloonNoteBuilder Created in NX6.0.0 |
interface |
BaseSurfaceFinish
Represents a Base Surface Finish
This is an abstract class, and cannot be instantiated. |
interface |
CompanyProprietaryInformation
Represents a Company Proprietary Information
To create or edit an instance of this class, use CompanyProprietaryInformationBuilder Created in NX6.0.0 |
interface |
CoordinateNote
Represents a Coordinate Note
To create or edit an instance of this class, use CoordinateNoteBuilder Created in NX6.0.0 |
interface |
DraftingSurfaceFinish
Represents a Drafting Surface Finish
To create or edit an instance of this class, use DraftingSurfaceFinishBuilder Created in NX7.5.0 |
interface |
EnterpriseIdentification
Represents a Enterprise Identification
To create or edit an instance of this class, use EnterpriseIdentificationBuilder Created in NX6.0.0 |
interface |
ExportControl
Represents a Export Control
To create or edit an instance of this class, use ExportControlBuilder Created in NX6.0.0 |
interface |
GeneralNote
Represents a General Note
To create or edit an instance of this class, use GeneralNoteBuilder Created in NX6.0.0 |
interface |
GovernmentSecurityInformation
Represents a Government Security Information
To create or edit an instance of this class, use GovernmentSecurityInformationBuilder Created in NX6.0.0 |
interface |
LocatorDesignator
Represents a Locator Designator
To create or edit an instance of this class, use LocatorDesignatorBuilder Created in NX6.0.0 |
interface |
MaterialSpecification
Represents a Material Specification
To create or edit an instance of this class, use MaterialSpecificationBuilder Created in NX6.0.0 |
interface |
PartIdentification
Represents a Part Identification
To create or edit an instance of this class, use PartIdentificationBuilder Created in NX6.0.0 |
interface |
PmiInteger
Represents a Pmi Integer
To create or edit an instance of this class, use PmiIntegerBuilder Created in NX6.0.0 |
interface |
PmiNumber
Represents a Pmi Number
To create or edit an instance of this class, use PmiNumberBuilder Created in NX6.0.0 |
interface |
PmiString
Represents a Pmi String
To create or edit an instance of this class, use nxopen.annotations.PmiStringBuilder Created in NX6.0.0 |
interface |
PmiUrlNote
Represents a Pmi url Note
To create or edit an instance of this class, use PmiUrlNoteBuilder Created in NX6.0.0 |
interface |
PmiUserDefined
Represents a User Defined Attribute
To create or edit an instance of this class, use PmiUserDefinedBuilder Created in NX6.0.0 |
interface |
ProcessSpecification
Represents a Process Specification
To create or edit an instance of this class, use ProcessSpecificationBuilder Created in NX6.0.0 |
interface |
SpecificNote
Represents a Specific Note
To create or edit an instance of this class, use SpecificNoteBuilder Created in NX6.0.0 |
interface |
SurfaceFinish
Represents a PMI Surface Finish
To create or edit an instance of this class, use SurfaceFinishBuilder Created in NX6.0.0 |
Modifier and Type | Method and Description |
---|---|
PmiAttributeBuilder |
PmiAttributeCollection.createPmiAttributeBuilder(PmiAttribute pmiAttr)
Creates a
PmiAttributeBuilder
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.