Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static MaterialConditionModifier |
MaterialConditionModifier.LAST
Last enum value.
|
static MaterialConditionModifier |
MaterialConditionModifier.LMC
Specifies least material condition modifier
|
static MaterialConditionModifier |
MaterialConditionModifier.MMC
Specifies maximum material condition modifier
|
static MaterialConditionModifier |
MaterialConditionModifier.NONE
Specifies no material modifier.
|
static MaterialConditionModifier |
MaterialConditionModifier.RFS
Specified regardless of feature size modifier
|
static MaterialConditionModifier |
MaterialConditionModifier.TANGENTIAL
Specifies tangent plane modifier
|
Modifier and Type | Method and Description |
---|---|
MaterialConditionModifier[] |
FcfFrame.getMaterialConditionModifiers()
Deprecated.
Deprecated in NX10.0.0. Use
Annotations.FeatureControlFrameDataBuilder#materialModifier and Annotations.FeatureControlFrameDataBuilder#setMaterialModifier instead.
|
MaterialConditionModifier[] |
DatumReference.getMaterialConditionModifiers()
Returns the material condition modifiers
License requirements: None. |
static MaterialConditionModifier |
MaterialConditionModifier.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MaterialConditionModifier |
MaterialConditionModifier.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MaterialConditionModifier[] |
MaterialConditionModifier.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FcfFrame.setMaterialConditionModifiers(MaterialConditionModifier[] modifiers)
Deprecated.
Deprecated in NX10.0.0. Use
Annotations.FeatureControlFrameDataBuilder#materialModifier and Annotations.FeatureControlFrameDataBuilder#setMaterialModifier instead.
|
void |
DatumReference.setMaterialConditionModifiers(MaterialConditionModifier[] modifiers)
Sets the material condition modifiers
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.