public static class SketchConstraintBuilder.Constraint extends Enum
Modifier and Type | Method and Description |
---|---|
static SketchConstraintBuilder.Constraint |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchConstraintBuilder.Constraint |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchConstraintBuilder.Constraint[] |
values()
Returns an array that contains the values for this enum.
|
public static final SketchConstraintBuilder.Constraint COINCIDENT
public static final SketchConstraintBuilder.Constraint POINT_ON_CURVE
public static final SketchConstraintBuilder.Constraint TANGENT
public static final SketchConstraintBuilder.Constraint PARALLEL
public static final SketchConstraintBuilder.Constraint PERPENDICULAR
public static final SketchConstraintBuilder.Constraint HORIZONTAL
public static final SketchConstraintBuilder.Constraint VERTICAL
public static final SketchConstraintBuilder.Constraint MIDPOINT
public static final SketchConstraintBuilder.Constraint COLLINEAR
public static final SketchConstraintBuilder.Constraint CONCENTRIC
public static final SketchConstraintBuilder.Constraint EQUAL_LENGTH
public static final SketchConstraintBuilder.Constraint EQUAL_RADIUS
public static final SketchConstraintBuilder.Constraint SYMMETRIC
public static final SketchConstraintBuilder.Constraint FIXED
public static final SketchConstraintBuilder.Constraint FULLY_FIXED
public static final SketchConstraintBuilder.Constraint CONSTANT_ANGLE
public static final SketchConstraintBuilder.Constraint CONSTANT_LENGTH
public static final SketchConstraintBuilder.Constraint POINT_ON_STRING
public static final SketchConstraintBuilder.Constraint NON_UNIFORM_SCALE
public static final SketchConstraintBuilder.Constraint UNIFORM_SCALE
public static final SketchConstraintBuilder.Constraint SLOPE_OF_CURVE
public static final int _COINCIDENT
public static final int _POINT_ON_CURVE
public static final int _TANGENT
public static final int _PARALLEL
public static final int _PERPENDICULAR
public static final int _HORIZONTAL
public static final int _VERTICAL
public static final int _MIDPOINT
public static final int _COLLINEAR
public static final int _CONCENTRIC
public static final int _EQUAL_LENGTH
public static final int _EQUAL_RADIUS
public static final int _SYMMETRIC
public static final int _FIXED
public static final int _FULLY_FIXED
public static final int _CONSTANT_ANGLE
public static final int _CONSTANT_LENGTH
public static final int _POINT_ON_STRING
public static final int _NON_UNIFORM_SCALE
public static final int _UNIFORM_SCALE
public static final int _SLOPE_OF_CURVE
public static SketchConstraintBuilder.Constraint valueOf(int value)
public static SketchConstraintBuilder.Constraint valueOf(String name)
public static SketchConstraintBuilder.Constraint[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.