ToolingSession Class¶
-
class
NXOpen.Tooling.
ToolingSession
¶ Bases:
object
Represents Tooling session
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
ClosePart | Close an existing part |
CreateCloneObject | Creates the clone operation object @return the new NXOpen.Tooling.CloneObject instance |
CreateSpreadsheetData | Create Tooling. |
GetReusableComponent | Gets the reusable component @return The array of reuseable components |
GetReusableObjects | Gets the last added reusable object |
LoadReusablePart | Opens an existing part, but does not set it to be the displayed part. |
Method Detail¶
ClosePart¶
-
ToolingSession.
ClosePart
¶ Close an existing part
Signature
ClosePart(part, wholeTree, closeModified)
Parameters: - part (
NXOpen.NXObject
) – Tag of the part that will be closed - wholeTree (
NXOpen.BasePartCloseWholeTree
) – If true, unloads all components of the part. If false, unloads only the top-level part - closeModified (
NXOpen.BasePartCloseModified
) – Behavior of close if component parts are modified.
New in version NX9.0.2.
License requirements: None.
- part (
CreateCloneObject¶
-
ToolingSession.
CreateCloneObject
¶ Creates the clone operation object
Signature
CreateCloneObject(applicationType, cloneActionType)
Parameters: - applicationType (
NXOpen.Tooling.ToolingApplication
) – Application type to determine the clone settings - cloneActionType (
NXOpen.Tooling.ToolingCloneaction
) – Clone action type
Returns: the new
NXOpen.Tooling.CloneObject
instanceReturn type: New in version NX8.0.0.
License requirements: None.
- applicationType (
CreateSpreadsheetData¶
-
ToolingSession.
CreateSpreadsheetData
¶ Create Tooling.
SpreadsheetData object.
Signature
CreateSpreadsheetData()
Returns: the new NXOpen.Tooling.SpreadsheetData
instanceReturn type: NXOpen.Tooling.SpreadsheetData
New in version NX8.0.0.
License requirements: None.
GetReusableComponent¶
-
ToolingSession.
GetReusableComponent
¶ Gets the reusable component
Signature
GetReusableComponent()
Returns: The array of reuseable components Return type: list of NXOpen.Assemblies.Component
New in version NX9.0.0.
License requirements: None.
GetReusableObjects¶
-
ToolingSession.
GetReusableObjects
¶ Gets the last added reusable object
Signature
GetReusableObjects(part)
Parameters: part ( NXOpen.NXObject
) – Tag of the part that contains reusable objectsReturns: Objects, mainly bodies, from the input part Return type: list of NXOpen.NXObject
New in version NX10.0.0.
License requirements: None.
LoadReusablePart¶
-
ToolingSession.
LoadReusablePart
¶ Opens an existing part, but does not set it to be the displayed part.
Signature
LoadReusablePart(filename, isNativePart)
Parameters: - filename (str) – Name of part file NOTE: The full Unicode character set is not supported for this parameter.
- isNativePart (bool) – Is the file from native or TC
Returns: Part Tag
Return type: New in version NX9.0.1.
License requirements: None.