ToolingApplication Enumeration¶
-
class
NXOpen.Tooling.
ToolingApplication
¶ Bases:
object
Wizard type, some of them should be same as in mpdwshare_uf_mold.
h Enum Members
Enum Member Enum Member Description ReuseLibrary Reuse LibraryMoldWizard MoldWizardPdieWizard Progressive Die WizardStampingDie Stamping DieElectrodeWizard Electrode WizardEdieWizard Engineering Die Wizard-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-