SubInsertBuilder Class¶
-
class
NXOpen.Tooling.
SubInsertBuilder
¶ Bases:
NXOpen.Builder
The SubInsert builder
To create a new instance of this class, use
NXOpen.Tooling.SubInsertCollection.CreateSubInsertBuilder
Default values.
Property Value InputParm 0 Rename 0 SelFootType Box New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
InputParm | Returns or sets the parameter of foot |
Rename | Returns or sets the subinsert name |
SelFootType | Returns or sets the foot type which can be a box or a cylinder |
SelectBotFace | Returns the bottom face to position the sub-insert |
SelectHead | Returns the head of sub-insert |
Tag | Returns the Tag for this object. |
Type | Returns or sets the parent part type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditDatabase | Edit datebase of foot |
EditRegFile | Edit register file of foot |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubInsertBuilderShape Enumeration | Represents the foot shape |
SubInsertBuilderTypes Enumeration | Represents the type of parent part |
Property Detail¶
InputParm¶
-
SubInsertBuilder.
InputParm
¶ Returns or sets the parameter of foot
-------------------------------------
Getter Method
Signature
InputParm()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InputParm(inputParm)
Parameters: inputParm (float) – New in version NX6.0.0.
License requirements: None.
Rename¶
-
SubInsertBuilder.
Rename
¶ Returns or sets the subinsert name
-------------------------------------
Getter Method
Signature
Rename()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rename(rename)
Parameters: rename (bool) – New in version NX6.0.0.
License requirements: None.
SelFootType¶
-
SubInsertBuilder.
SelFootType
¶ Returns or sets the foot type which can be a box or a cylinder
-------------------------------------
Getter Method
Signature
SelFootType()
Returns: Return type: NXOpen.Tooling.SubInsertBuilderShape
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelFootType(selFootType)
Parameters: selFootType ( NXOpen.Tooling.SubInsertBuilderShape
) –New in version NX6.0.0.
License requirements: None.
SelectBotFace¶
-
SubInsertBuilder.
SelectBotFace
¶ Returns the bottom face to position the sub-insert
-------------------------------------
Getter Method
Signature
SelectBotFace()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
SelectHead¶
-
SubInsertBuilder.
SelectHead
¶ Returns the head of sub-insert
-------------------------------------
Getter Method
Signature
SelectHead()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
Type¶
-
SubInsertBuilder.
Type
¶ Returns or sets the parent part type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.SubInsertBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.SubInsertBuilderTypes
) –New in version NX8.0.0.
License requirements: None.
Method Detail¶
EditDatabase¶
-
SubInsertBuilder.
EditDatabase
¶ Edit datebase of foot
Signature
EditDatabase()
New in version NX6.0.0.
License requirements: None.
EditRegFile¶
-
SubInsertBuilder.
EditRegFile
¶ Edit register file of foot
Signature
EditRegFile()
New in version NX6.0.0.
License requirements: None.
Validate¶
-
SubInsertBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.