SubInsertBuilderTypes Enumeration¶
NXOpen.Tooling.SubInsertBuilder.Types is an alias for NXOpen.Tooling.SubInsertBuilderTypes
-
class
NXOpen.Tooling.
SubInsertBuilderTypes
¶ Bases:
object
Represents the type of parent part
Enum Members
Enum Member Enum Member Description ParentOfSolidOwningPart The parent part is the parent of solid owning partProdPart The parent part is Prod partSolidOwningPart The parent part is the owning part of solidCurrentWorkPart The parent part is current work part-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-