MWDefineRegionsBuilder Class¶
-
class
NXOpen.Tooling.
MWDefineRegionsBuilder
¶ Bases:
NXOpen.Builder
The MWDefineRegions builder
To create a new instance of this class, use
NXOpen.Tooling.MWDefineRegionsCollection.CreateBuilder
Default values.
Property Value CreatePartingLinesToggle 0 CreateRegionsToggle 0 TranslucencyOption SelectedFaces TranslucencyValueScale 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CreatePartingLinesToggle | Returns or sets the create parting lines toggle |
CreateRegionsToggle | Returns or sets the create regions toggle |
FaceColor | Returns or sets the face color for the selected region faces |
SelectRegionFaces | Returns the region faces for defining region |
Tag | Returns the Tag for this object. |
TranslucencyOption | Returns or sets the translucency option for the selected or non-selected region faces |
TranslucencyValueScale | Returns or sets the translucency value for the selected or non-selected region faces |
Methods¶
Method | Description |
---|---|
ChangeCurrentRegionName | Change the region name for the current region @return return status |
ChangeEntitiesColor | Change the color of displayable entities |
ChangeRegionFacesColor | Change the color of the faces of a region |
ChangeRegionLayer | Change the layer of the region |
Commit | Commits any edits that have been applied to the builder. |
CreateNewRegion | Create a new region @return new region object created |
CreateNewRegionButton | Button to create a new empty region |
DeleteAllExistingRegions | Delete all existing regions |
DeleteRegion | Delete a region |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisplayProductBody | Display the product body in the part file |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOrCreateEmptyRegion | Get or create an empty region @return empty region object |
HookupRegionUdoAndBodyForCavityAndCore | Hook up cavity and core region UDO objects with the corresponding sheet bodies |
SearchRegionButton | Button to invoke searching region |
SetCurrentRegion | Set the current region |
SetupRegionsInfo | Setup the UI data for defining regions |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateUndefinedFaces | Update the undefined faces |
UpdateUnsewnBodiesNameAttribute | Update name attribute for the unsew bodies of the cavity and core regions |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MWDefineRegionsBuilderTranslucencyOptionType Enumeration | This enum represents the translucency is to be performed on the selected or non-selected region faces |
Property Detail¶
CreatePartingLinesToggle¶
-
MWDefineRegionsBuilder.
CreatePartingLinesToggle
¶ Returns or sets the create parting lines toggle
-------------------------------------
Getter Method
Signature
CreatePartingLinesToggle()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreatePartingLinesToggle(createPartingLinesToggle)
Parameters: createPartingLinesToggle (bool) – New in version NX6.0.0.
License requirements: None.
CreateRegionsToggle¶
-
MWDefineRegionsBuilder.
CreateRegionsToggle
¶ Returns or sets the create regions toggle
-------------------------------------
Getter Method
Signature
CreateRegionsToggle()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateRegionsToggle(createRegionsToggle)
Parameters: createRegionsToggle (bool) – New in version NX6.0.0.
License requirements: None.
FaceColor¶
-
MWDefineRegionsBuilder.
FaceColor
¶ Returns or sets the face color for the selected region faces
-------------------------------------
Getter Method
Signature
FaceColor()
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceColor(faceColor)
Parameters: faceColor (Id) – New in version NX6.0.0.
License requirements: None.
SelectRegionFaces¶
-
MWDefineRegionsBuilder.
SelectRegionFaces
¶ Returns the region faces for defining region
-------------------------------------
Getter Method
Signature
SelectRegionFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
TranslucencyOption¶
-
MWDefineRegionsBuilder.
TranslucencyOption
¶ Returns or sets the translucency option for the selected or non-selected region faces
-------------------------------------
Getter Method
Signature
TranslucencyOption()
Returns: Return type: NXOpen.Tooling.MWDefineRegionsBuilderTranslucencyOptionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TranslucencyOption(translucencyOption)
Parameters: translucencyOption ( NXOpen.Tooling.MWDefineRegionsBuilderTranslucencyOptionType
) –New in version NX6.0.0.
License requirements: None.
TranslucencyValueScale¶
-
MWDefineRegionsBuilder.
TranslucencyValueScale
¶ Returns or sets the translucency value for the selected or non-selected region faces
-------------------------------------
Getter Method
Signature
TranslucencyValueScale()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TranslucencyValueScale(translucencyValueScale)
Parameters: translucencyValueScale (int) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
ChangeCurrentRegionName¶
-
MWDefineRegionsBuilder.
ChangeCurrentRegionName
¶ Change the region name for the current region
Signature
ChangeCurrentRegionName(regionName)
Parameters: regionName (str) – region name Returns: return status Return type: int New in version NX6.0.3.
License requirements: None.
ChangeEntitiesColor¶
-
MWDefineRegionsBuilder.
ChangeEntitiesColor
¶ Change the color of displayable entities
Signature
ChangeEntitiesColor(entities, color)
Parameters: - entities (list of
NXOpen.TaggedObject
) – an array of entities - color (int) – color for entities
New in version NX6.0.3.
License requirements: None.
- entities (list of
ChangeRegionFacesColor¶
-
MWDefineRegionsBuilder.
ChangeRegionFacesColor
¶ Change the color of the faces of a region
Signature
ChangeRegionFacesColor(regionName, allOrUndefined, color)
Parameters: - regionName (str) – region name
- allOrUndefined (int) – 1: All faces, 2: Undefined faces when regionUDO is 0
- color (int) – color for region faces
New in version NX6.0.3.
License requirements: None.
ChangeRegionLayer¶
-
MWDefineRegionsBuilder.
ChangeRegionLayer
¶ Change the layer of the region
Signature
ChangeRegionLayer(regionName, layer)
Parameters: - regionName (str) – region name
- layer (int) – layer for region faces
New in version NX6.0.3.
License requirements: None.
CreateNewRegion¶
-
MWDefineRegionsBuilder.
CreateNewRegion
¶ Create a new region
Signature
CreateNewRegion()
Returns: new region object created Return type: str New in version NX6.0.3.
License requirements: None.
CreateNewRegionButton¶
-
MWDefineRegionsBuilder.
CreateNewRegionButton
¶ Button to create a new empty region
Signature
CreateNewRegionButton()
New in version NX6.0.0.
License requirements: None.
DeleteAllExistingRegions¶
-
MWDefineRegionsBuilder.
DeleteAllExistingRegions
¶ Delete all existing regions
Signature
DeleteAllExistingRegions()
New in version NX6.0.3.
License requirements: None.
DeleteRegion¶
-
MWDefineRegionsBuilder.
DeleteRegion
¶ Delete a region
Signature
DeleteRegion(regionName)
Parameters: regionName (str) – region object to be deleted New in version NX6.0.3.
License requirements: None.
DisplayProductBody¶
-
MWDefineRegionsBuilder.
DisplayProductBody
¶ Display the product body in the part file
Signature
DisplayProductBody()
New in version NX6.0.3.
License requirements: None.
GetOrCreateEmptyRegion¶
-
MWDefineRegionsBuilder.
GetOrCreateEmptyRegion
¶ Get or create an empty region
Signature
GetOrCreateEmptyRegion()
Returns: a tuple Return type: A tuple consisting of (regionName, created). regionName is a str. empty region object created is a int. Return flag indicating if an empty region UDO is created New in version NX6.0.3.
License requirements: None.
HookupRegionUdoAndBodyForCavityAndCore¶
-
MWDefineRegionsBuilder.
HookupRegionUdoAndBodyForCavityAndCore
¶ Hook up cavity and core region UDO objects with the corresponding sheet bodies
Signature
HookupRegionUdoAndBodyForCavityAndCore()
New in version NX6.0.3.
License requirements: None.
SearchRegionButton¶
-
MWDefineRegionsBuilder.
SearchRegionButton
¶ Button to invoke searching region
Signature
SearchRegionButton()
New in version NX6.0.0.
License requirements: None.
SetCurrentRegion¶
-
MWDefineRegionsBuilder.
SetCurrentRegion
¶ Set the current region
Signature
SetCurrentRegion(regionName)
Parameters: regionName (str) – current region name New in version NX6.0.3.
License requirements: None.
SetupRegionsInfo¶
-
MWDefineRegionsBuilder.
SetupRegionsInfo
¶ Setup the UI data for defining regions
Signature
SetupRegionsInfo()
New in version NX6.0.3.
License requirements: None.
UpdateUndefinedFaces¶
-
MWDefineRegionsBuilder.
UpdateUndefinedFaces
¶ Update the undefined faces
Signature
UpdateUndefinedFaces(changeColor)
Parameters: changeColor (int) – indicator for changing color too New in version NX6.0.3.
License requirements: None.
UpdateUnsewnBodiesNameAttribute¶
-
MWDefineRegionsBuilder.
UpdateUnsewnBodiesNameAttribute
¶ Update name attribute for the unsew bodies of the cavity and core regions
Signature
UpdateUnsewnBodiesNameAttribute(unsewFeatureTag, cavityFaces)
Parameters: - unsewFeatureTag (
NXOpen.TaggedObject
) – Unsewn feature object - cavityFaces (list of
NXOpen.Face
) – an array of cavity faces
New in version NX6.0.3.
License requirements: None.
- unsewFeatureTag (
Validate¶
-
MWDefineRegionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.