MWDefineRegionsBuilderTranslucencyOptionType Enumeration¶
NXOpen.Tooling.MWDefineRegionsBuilder.TranslucencyOptionType is an alias for NXOpen.Tooling.MWDefineRegionsBuilderTranslucencyOptionType
-
class
NXOpen.Tooling.
MWDefineRegionsBuilderTranslucencyOptionType
¶ Bases:
object
This enum represents the translucency is to be performed on the selected or non-selected region faces
Enum Members
Enum Member Enum Member Description SelectedFaces Selected region facesOtherFaces Non-selected region faces-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-