HoleReportBuilder Class¶
-
class
NXOpen.Tooling.
HoleReportBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.HoleReportBuilder
This class is for Hole Report Design UITo create a new instance of this class, use
NXOpen.Tooling.HoleReportCollection.CreateHoleReportBuilder
Default values.
Property Value QuadrantType PositiveQuadrantI SelectionType ViewSelection New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CreatedOrdinateOrigin | Returns or sets the created ordinate origin |
HoleTable | Returns the hole table to edit |
OrdinateOrigin | Returns the ordinate origin to get the coords in given ordinate |
QuadrantType | Returns or sets the positive quadrant type |
SelectionType | Returns or sets the selection type to choose select view or holes in window to create hole report |
TableAddHole | Returns the holes to add to the table |
TableHole | Returns the holes in window to create hole report |
TableOrigin | Returns or sets the table origin |
TableView | Returns the view to create hole report |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of hole table |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateOrdinateOrigin | Create Ordinate Origin @return the new ordinate |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HoleReportBuilderEnumQuadrantType Enumeration | Specifies the option of which quadrant is positive |
HoleReportBuilderEnumSelectionType Enumeration | Specifies the option of selection type to create hole table |
HoleReportBuilderTypes Enumeration | Specifies the option of hole table type |
Property Detail¶
CreatedOrdinateOrigin¶
-
HoleReportBuilder.
CreatedOrdinateOrigin
¶ Returns or sets the created ordinate origin
-------------------------------------
Getter Method
Signature
CreatedOrdinateOrigin()
Returns: Returns the created ordinate origin Return type: NXOpen.TaggedObject
New in version NX6.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreatedOrdinateOrigin(ordinateOriginTag)
Parameters: ordinateOriginTag ( NXOpen.TaggedObject
) – Sets the created ordinate originNew in version NX6.0.3.
License requirements: None.
HoleTable¶
-
HoleReportBuilder.
HoleTable
¶ Returns the hole table to edit
-------------------------------------
Getter Method
Signature
HoleTable()
Returns: Returns the hole table to edit Return type: NXOpen.SelectEdgeList
New in version NX6.0.0.
License requirements: None.
OrdinateOrigin¶
-
HoleReportBuilder.
OrdinateOrigin
¶ Returns the ordinate origin to get the coords in given ordinate
-------------------------------------
Getter Method
Signature
OrdinateOrigin()
Returns: Returns the edge in which the ordinate origin is Return type: NXOpen.SelectPointList
New in version NX6.0.0.
License requirements: None.
QuadrantType¶
-
HoleReportBuilder.
QuadrantType
¶ Returns or sets the positive quadrant type
-------------------------------------
Getter Method
Signature
QuadrantType()
Returns: Returns the positive quadrant type Return type: NXOpen.Tooling.HoleReportBuilderEnumQuadrantType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QuadrantType(quadrantType)
Parameters: quadrantType ( NXOpen.Tooling.HoleReportBuilderEnumQuadrantType
) – Sets the positive quadrant typeNew in version NX6.0.0.
License requirements: None.
SelectionType¶
-
HoleReportBuilder.
SelectionType
¶ Returns or sets the selection type to choose select view or holes in window to create hole report
-------------------------------------
Getter Method
Signature
SelectionType()
Returns: Returns the selection type value Return type: NXOpen.Tooling.HoleReportBuilderEnumSelectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionType(selectionType)
Parameters: selectionType ( NXOpen.Tooling.HoleReportBuilderEnumSelectionType
) – Sets the selection type valueNew in version NX6.0.0.
License requirements: None.
TableAddHole¶
-
HoleReportBuilder.
TableAddHole
¶ Returns the holes to add to the table
-------------------------------------
Getter Method
Signature
TableAddHole()
Returns: Returns the holes to add to the table Return type: NXOpen.SelectEdgeList
New in version NX6.0.0.
License requirements: None.
TableHole¶
-
HoleReportBuilder.
TableHole
¶ Returns the holes in window to create hole report
-------------------------------------
Getter Method
Signature
TableHole()
Returns: Returns the holes in window to create hole table Return type: NXOpen.SelectEdgeList
New in version NX6.0.0.
License requirements: None.
TableOrigin¶
-
HoleReportBuilder.
TableOrigin
¶ Returns or sets the table origin
-------------------------------------
Getter Method
Signature
TableOrigin()
Returns: Returns the table origin to create hole table Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TableOrigin(tableOrigin)
Parameters: tableOrigin ( NXOpen.Point
) – Sets the table origin to create hole tableNew in version NX6.0.0.
License requirements: None.
TableView¶
-
HoleReportBuilder.
TableView
¶ Returns the view to create hole report
-------------------------------------
Getter Method
Signature
TableView()
Returns: Returns the view to create hole table Return type: NXOpen.Drawings.SelectDraftingViewList
New in version NX6.0.0.
License requirements: None.
Type¶
-
HoleReportBuilder.
Type
¶ Returns or sets the type of hole table
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.HoleReportBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.HoleReportBuilderTypes
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreateOrdinateOrigin¶
-
HoleReportBuilder.
CreateOrdinateOrigin
¶ Create Ordinate Origin
Signature
CreateOrdinateOrigin(quadrant, viewTag, pointData)
Parameters: - quadrant (int) – value of the positive quadrant
- viewTag (
NXOpen.TaggedObject
) – the view - pointData (
NXOpen.Point3d
) – data of the cursor point
Returns: the new ordinate
Return type: New in version NX6.0.3.
License requirements: None.
Validate¶
-
HoleReportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.