HoleReportBuilderEnumSelectionType Enumeration¶
NXOpen.Tooling.HoleReportBuilder.EnumSelectionType is an alias for NXOpen.Tooling.HoleReportBuilderEnumSelectionType
-
class
NXOpen.Tooling.
HoleReportBuilderEnumSelectionType
¶ Bases:
object
Specifies the option of selection type to create hole table
Enum Members
Enum Member Enum Member Description ViewSelection Selects view to create hole tableWindowSelection Selects holes in window to create hole table-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-