FormingInsertBuilder Class¶
-
class
NXOpen.Tooling.
FormingInsertBuilder
¶ Bases:
NXOpen.Builder
Progressive Die Wizard builder to design forming punch and die insert
To create a new instance of this class, use
NXOpen.Tooling.FormingInsertCollection.CreateFormingInsertBuilder
Default values.
Property Value AngleToleranceValue 45 BlankPosition PunchPlate BlankType Standard BottomPlateClearance 0 DesignOption FormingPunch DiePlateClearance 0 HeightValue.Value 0 (millimeters part), 0 (inches part) ParentPart DieBase PunchPlateClearance 0 SameWithPlate 0 StripperPlateClearance 0 TangentEdgeAngle 0 TraverseInteriorEdges 0 UseBottomPlateClearance 0 UseDiePlateClearance 0 UsePunchPlateClearance 0 UseStripperPlateClearance 0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AngleToleranceValue | Returns or sets the tangent edge angle tolerance value of forming region. |
BlankPosition | Returns or sets the blank position in punch plate or stripper plate. |
BlankProfile | Returns the blank profile to extrude the punch or die. |
BlankType | Returns or sets the blank type for punch or die. |
BottomPlateClearance | Returns or sets the clearance value of bottom backing plate . |
BoundaryFaces | Returns the boundary faces of forming region. |
DesignOption | Returns or sets the design option to design punch or die. |
DiePlateClearance | Returns or sets the clearance value of die plate. |
HeightValue | Returns the height value of blank. |
LowerValue | Returns the lower value of blank. |
ParentPart | Returns or sets the parent part to create blank. |
ParentPartName | Returns or sets the parent part name to create blank. |
PunchOrDieToEdit | Returns the punch or die to edit |
PunchPlateClearance | Returns or sets the clearance value of punch plate . |
RenameComponent | Returns or sets the option whether rename component. |
ReverseDirection | Returns or sets the option to reverse trim direction. |
SameWithPlate | Returns or sets the punch same with plate |
SeedFace | Returns the seed face of forming region. |
SelectFormingFaces | Returns the forming faces of forming region. |
StripperPlateClearance | Returns or sets the option to use the stripper plate clearance. |
Tag | Returns the Tag for this object. |
TangentEdgeAngle | Returns or sets the tangent edge angle of forming region. |
TraverseInteriorEdges | Returns or sets the indication to traverse interior edges of forming region. |
UseBottomPlateClearance | Returns or sets the option to use bottom backing plate clearance. |
UseDiePlateClearance | Returns or sets the option to use die plate clearance. |
UsePunchPlateClearance | Returns or sets the option to use punch plate clearance. |
UseStripperPlateClearance | Returns or sets the option to use stripper plate clearance. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateNewComponent | Create new component. |
DeletePunchOrDieComponent | The action to delete the selected punch or die component |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExtractFormingRegion | Extract forming region. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ReverseTrimDirection | Reverse trim direction. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FormingInsertBuilderBlankPositions Enumeration | Specifies the blank position. |
FormingInsertBuilderBlankTypes Enumeration | Specifies the blank type. |
FormingInsertBuilderDesignOptions Enumeration | Specifies the design type. |
FormingInsertBuilderParentTypes Enumeration | Specifies the parent part type. |
Property Detail¶
AngleToleranceValue¶
-
FormingInsertBuilder.
AngleToleranceValue
¶ Returns or sets the tangent edge angle tolerance value of forming region.
-------------------------------------
Getter Method
Signature
AngleToleranceValue()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleToleranceValue(angleToleranceValue)
Parameters: angleToleranceValue (float) – New in version NX7.5.0.
License requirements: None.
BlankPosition¶
-
FormingInsertBuilder.
BlankPosition
¶ Returns or sets the blank position in punch plate or stripper plate.
-------------------------------------
Getter Method
Signature
BlankPosition()
Returns: Return type: NXOpen.Tooling.FormingInsertBuilderBlankPositions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankPosition(blankPosition)
Parameters: blankPosition ( NXOpen.Tooling.FormingInsertBuilderBlankPositions
) –New in version NX7.5.0.
License requirements: None.
BlankProfile¶
-
FormingInsertBuilder.
BlankProfile
¶ Returns the blank profile to extrude the punch or die.
-------------------------------------
Getter Method
Signature
BlankProfile()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
BlankType¶
-
FormingInsertBuilder.
BlankType
¶ Returns or sets the blank type for punch or die.
-------------------------------------
Getter Method
Signature
BlankType()
Returns: Return type: NXOpen.Tooling.FormingInsertBuilderBlankTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankType(blankType)
Parameters: blankType ( NXOpen.Tooling.FormingInsertBuilderBlankTypes
) –New in version NX7.5.0.
License requirements: None.
BottomPlateClearance¶
-
FormingInsertBuilder.
BottomPlateClearance
¶ Returns or sets the clearance value of bottom backing plate .
-------------------------------------
Getter Method
Signature
BottomPlateClearance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BottomPlateClearance(bottomPlateClr)
Parameters: bottomPlateClr (float) – New in version NX7.5.0.
License requirements: None.
BoundaryFaces¶
-
FormingInsertBuilder.
BoundaryFaces
¶ Returns the boundary faces of forming region.
-------------------------------------
Getter Method
Signature
BoundaryFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
DesignOption¶
-
FormingInsertBuilder.
DesignOption
¶ Returns or sets the design option to design punch or die.
-------------------------------------
Getter Method
Signature
DesignOption()
Returns: Return type: NXOpen.Tooling.FormingInsertBuilderDesignOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignOption(designOption)
Parameters: designOption ( NXOpen.Tooling.FormingInsertBuilderDesignOptions
) –New in version NX7.5.0.
License requirements: None.
DiePlateClearance¶
-
FormingInsertBuilder.
DiePlateClearance
¶ Returns or sets the clearance value of die plate.
-------------------------------------
Getter Method
Signature
DiePlateClearance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiePlateClearance(diePlateClr)
Parameters: diePlateClr (float) – New in version NX7.5.0.
License requirements: None.
HeightValue¶
-
FormingInsertBuilder.
HeightValue
¶ Returns the height value of blank.
-------------------------------------
Getter Method
Signature
HeightValue()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
LowerValue¶
-
FormingInsertBuilder.
LowerValue
¶ Returns the lower value of blank.
-------------------------------------
Getter Method
Signature
LowerValue()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ParentPart¶
-
FormingInsertBuilder.
ParentPart
¶ Returns or sets the parent part to create blank.
-------------------------------------
Getter Method
Signature
ParentPart()
Returns: Return type: NXOpen.Tooling.FormingInsertBuilderParentTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPart(parentPart)
Parameters: parentPart ( NXOpen.Tooling.FormingInsertBuilderParentTypes
) –New in version NX7.5.0.
License requirements: None.
ParentPartName¶
-
FormingInsertBuilder.
ParentPartName
¶ Returns or sets the parent part name to create blank.
-------------------------------------
Getter Method
Signature
ParentPartName()
Returns: Retruns parent part name Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPartName(parentPart)
Parameters: parentPart (str) – Specifies the parent part name New in version NX7.5.0.
License requirements: None.
PunchOrDieToEdit¶
-
FormingInsertBuilder.
PunchOrDieToEdit
¶ Returns the punch or die to edit
-------------------------------------
Getter Method
Signature
PunchOrDieToEdit()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
PunchPlateClearance¶
-
FormingInsertBuilder.
PunchPlateClearance
¶ Returns or sets the clearance value of punch plate .
-------------------------------------
Getter Method
Signature
PunchPlateClearance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchPlateClearance(punchPlateClr)
Parameters: punchPlateClr (float) – New in version NX7.5.0.
License requirements: None.
RenameComponent¶
-
FormingInsertBuilder.
RenameComponent
¶ Returns or sets the option whether rename component.
-------------------------------------
Getter Method
Signature
RenameComponent()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenameComponent(renameComponent)
Parameters: renameComponent (bool) – New in version NX8.5.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ReverseDirection¶
-
FormingInsertBuilder.
ReverseDirection
¶ Returns or sets the option to reverse trim direction.
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX7.5.0.
License requirements: None.
SameWithPlate¶
-
FormingInsertBuilder.
SameWithPlate
¶ Returns or sets the punch same with plate
-------------------------------------
Getter Method
Signature
SameWithPlate()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SameWithPlate(sameWithPlate)
Parameters: sameWithPlate (bool) – New in version NX7.5.0.
License requirements: None.
SeedFace¶
-
FormingInsertBuilder.
SeedFace
¶ Returns the seed face of forming region.
-------------------------------------
Getter Method
Signature
SeedFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
SelectFormingFaces¶
-
FormingInsertBuilder.
SelectFormingFaces
¶ Returns the forming faces of forming region.
-------------------------------------
Getter Method
Signature
SelectFormingFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
StripperPlateClearance¶
-
FormingInsertBuilder.
StripperPlateClearance
¶ Returns or sets the option to use the stripper plate clearance.
-------------------------------------
Getter Method
Signature
StripperPlateClearance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StripperPlateClearance(stripperPlateClr)
Parameters: stripperPlateClr (float) – New in version NX7.5.0.
License requirements: None.
TangentEdgeAngle¶
-
FormingInsertBuilder.
TangentEdgeAngle
¶ Returns or sets the tangent edge angle of forming region.
-------------------------------------
Getter Method
Signature
TangentEdgeAngle()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TangentEdgeAngle(tangentEdgeAngle)
Parameters: tangentEdgeAngle (bool) – New in version NX7.5.0.
License requirements: None.
TraverseInteriorEdges¶
-
FormingInsertBuilder.
TraverseInteriorEdges
¶ Returns or sets the indication to traverse interior edges of forming region.
-------------------------------------
Getter Method
Signature
TraverseInteriorEdges()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TraverseInteriorEdges(traverseInteriorEdges)
Parameters: traverseInteriorEdges (bool) – New in version NX7.5.0.
License requirements: None.
UseBottomPlateClearance¶
-
FormingInsertBuilder.
UseBottomPlateClearance
¶ Returns or sets the option to use bottom backing plate clearance.
-------------------------------------
Getter Method
Signature
UseBottomPlateClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseBottomPlateClearance(useBPClearance)
Parameters: useBPClearance (bool) – New in version NX7.5.0.
License requirements: None.
UseDiePlateClearance¶
-
FormingInsertBuilder.
UseDiePlateClearance
¶ Returns or sets the option to use die plate clearance.
-------------------------------------
Getter Method
Signature
UseDiePlateClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseDiePlateClearance(useDPClearance)
Parameters: useDPClearance (bool) – New in version NX7.5.0.
License requirements: None.
UsePunchPlateClearance¶
-
FormingInsertBuilder.
UsePunchPlateClearance
¶ Returns or sets the option to use punch plate clearance.
-------------------------------------
Getter Method
Signature
UsePunchPlateClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsePunchPlateClearance(usePPClearance)
Parameters: usePPClearance (bool) – New in version NX7.5.0.
License requirements: None.
UseStripperPlateClearance¶
-
FormingInsertBuilder.
UseStripperPlateClearance
¶ Returns or sets the option to use stripper plate clearance.
-------------------------------------
Getter Method
Signature
UseStripperPlateClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseStripperPlateClearance(useSPClearance)
Parameters: useSPClearance (bool) – New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreateNewComponent¶
-
FormingInsertBuilder.
CreateNewComponent
¶ Create new component.
Signature
CreateNewComponent(parentTag, origin)
Parameters: - parentTag (
NXOpen.TaggedObject
) – the parent part - origin (
NXOpen.Point3d
) – the origin point to add
Returns: the new part instance
Return type: New in version NX7.5.0.
License requirements: None.
- parentTag (
DeletePunchOrDieComponent¶
-
FormingInsertBuilder.
DeletePunchOrDieComponent
¶ The action to delete the selected punch or die component
Signature
DeletePunchOrDieComponent()
New in version NX7.5.0.
License requirements: None.
ExtractFormingRegion¶
-
FormingInsertBuilder.
ExtractFormingRegion
¶ Extract forming region.
Signature
ExtractFormingRegion()
New in version NX7.5.0.
License requirements: None.
ReverseTrimDirection¶
-
FormingInsertBuilder.
ReverseTrimDirection
¶ Reverse trim direction.
Signature
ReverseTrimDirection()
New in version NX7.5.0.
License requirements: None.
Validate¶
-
FormingInsertBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.