FormingInsertBuilderBlankPositions Enumeration¶
NXOpen.Tooling.FormingInsertBuilder.BlankPositions is an alias for NXOpen.Tooling.FormingInsertBuilderBlankPositions
-
class
NXOpen.Tooling.
FormingInsertBuilderBlankPositions
¶ Bases:
object
Specifies the blank position.
Enum Members
Enum Member Enum Member Description PunchPlate the blank is on the punch plateStripperPlate the blank is on the stripper plateDiePlate the blank is on the die plate-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-