BendInsertDesignBuilder Class¶
-
class
NXOpen.Tooling.
BendInsertDesignBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.BendInsertDesignBuilder
Bend Insert Design is to create inset puch or die for bend .To create a new instance of this class, use
NXOpen.Tooling.BendInsertDesignCollection.CreateBendInsertDesignBuilder
Default values.
Property Value BendType Sbend BendingDirection Down BlankPosition PunchPlate BottomPlateClearance 0 CompositeInsert 0 ConceptDesign 0 DiePlateClearance 0 Extend.Value 5 (millimeters part), 1 (inches part) ExtrudeEnd.Value 5 (millimeters part), 1 (inches part) ExtrudeStart.Value 0 (millimeters part), 0 (inches part) FalseBody 0 InsertType Punch ParentNode Sub PunchPlateClearance 0 ReName 0 StripperPlateClearance 0 Type Standard UseBottomPlateClearance 0 UseDiePlateClearance 0 UsePunchPlateClearance 0 UseStripperPlateClearance 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BendFace | Returns the bend face. |
BendType | Returns or sets the bend type. |
BendingDirection | Returns or sets the bending direction. |
BlankPosition | Returns or sets the blank position in punch plate or stripper plate. |
BottomPlateClearance | Returns or sets the clearance value of bottom backing plate. |
CompositeInsert | Returns or sets the composite insert. |
ConceptDesign | Returns or sets the concept design option. |
DiePlateClearance | Returns or sets the clearance value of die plate. |
Extend | Returns the extend. |
ExtrudeEnd | Returns the extrude end, A half when composite insert. |
ExtrudeEnd1 | Returns the extrude end B -half. |
ExtrudeSketch | Returns the extrude sketch. |
ExtrudeStart | Returns the extrude start, A half when composite insert. |
ExtrudeStart1 | Returns the extrude start - B half. |
FalseBody | Returns or sets the false body creation option. |
FlipTrimDirection | Returns or sets the flip trim feature direction of insert. |
InsertComponent | Returns the select insert to delete |
InsertToEdit | Returns the select insert to edit |
InsertType | Returns or sets the insert type. |
IntersectPlane | Returns or sets the intersect plane. |
IsAutoDatum | Returns or sets the auto datum plane |
NewPartName | Returns or sets the new component name. |
ParentNode | Returns or sets the parent node. |
ParentPartName | Returns or sets the parent part name to create insert. |
PunchPlateClearance | Returns or sets the clearance value of punch plate. |
ReName | Returns or sets the rename option. |
StripperPlateClearance | Returns or sets the clearance value of stripper plate. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the operation type of bending insert design. |
UseBottomPlateClearance | Returns or sets the option to use bottom backing plate clearance. |
UseDiePlateClearance | Returns or sets the option to use die plate clearance. |
UsePunchPlateClearance | Returns or sets the option to use punch plate clearance. |
UseStripperPlateClearance | Returns or sets the option to use stripper plate clearance. |
Methods¶
Method | Description |
---|---|
AddInsertComponent | Add the new bend insert component |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetFaces | Sets the face occurrences into builder attribute. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BendInsertDesignBuilderBendTypeOption Enumeration | the bend type. |
BendInsertDesignBuilderBendingDirectionOption Enumeration | the bending direction. |
BendInsertDesignBuilderBlankPositions Enumeration | Specifies the blank position. |
BendInsertDesignBuilderInsertTypeOption Enumeration | the insert type. |
BendInsertDesignBuilderParentOption Enumeration | the parent node. |
BendInsertDesignBuilderTypes Enumeration | the bending operation. |
Property Detail¶
BendFace¶
-
BendInsertDesignBuilder.
BendFace
¶ Returns the bend face.
-------------------------------------
Getter Method
Signature
BendFace()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
BendType¶
-
BendInsertDesignBuilder.
BendType
¶ Returns or sets the bend type.
-------------------------------------
Getter Method
Signature
BendType()
Returns: Return type: NXOpen.Tooling.BendInsertDesignBuilderBendTypeOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendType(bendType)
Parameters: bendType ( NXOpen.Tooling.BendInsertDesignBuilderBendTypeOption
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
BendingDirection¶
-
BendInsertDesignBuilder.
BendingDirection
¶ Returns or sets the bending direction.
-------------------------------------
Getter Method
Signature
BendingDirection()
Returns: Return type: NXOpen.Tooling.BendInsertDesignBuilderBendingDirectionOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendingDirection(bendingDirection)
Parameters: bendingDirection ( NXOpen.Tooling.BendInsertDesignBuilderBendingDirectionOption
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
BlankPosition¶
-
BendInsertDesignBuilder.
BlankPosition
¶ Returns or sets the blank position in punch plate or stripper plate.
-------------------------------------
Getter Method
Signature
BlankPosition()
Returns: Return type: NXOpen.Tooling.BendInsertDesignBuilderBlankPositions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankPosition(blankPosition)
Parameters: blankPosition ( NXOpen.Tooling.BendInsertDesignBuilderBlankPositions
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
BottomPlateClearance¶
-
BendInsertDesignBuilder.
BottomPlateClearance
¶ Returns or sets the clearance value of bottom backing plate.
-------------------------------------
Getter Method
Signature
BottomPlateClearance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BottomPlateClearance(bottomPlateClr)
Parameters: bottomPlateClr (float) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
CompositeInsert¶
-
BendInsertDesignBuilder.
CompositeInsert
¶ Returns or sets the composite insert.
-------------------------------------
Getter Method
Signature
CompositeInsert()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CompositeInsert(compositeInsert)
Parameters: compositeInsert (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ConceptDesign¶
-
BendInsertDesignBuilder.
ConceptDesign
¶ Returns or sets the concept design option.
-------------------------------------
Getter Method
Signature
ConceptDesign()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConceptDesign(conceptDesign)
Parameters: conceptDesign (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
DiePlateClearance¶
-
BendInsertDesignBuilder.
DiePlateClearance
¶ Returns or sets the clearance value of die plate.
-------------------------------------
Getter Method
Signature
DiePlateClearance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiePlateClearance(diePlateClr)
Parameters: diePlateClr (float) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Extend¶
-
BendInsertDesignBuilder.
Extend
¶ Returns the extend.
-------------------------------------
Getter Method
Signature
Extend()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ExtrudeEnd¶
-
BendInsertDesignBuilder.
ExtrudeEnd
¶ Returns the extrude end, A half when composite insert.
-------------------------------------
Getter Method
Signature
ExtrudeEnd()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ExtrudeEnd1¶
-
BendInsertDesignBuilder.
ExtrudeEnd1
¶ Returns the extrude end B -half.
-------------------------------------
Getter Method
Signature
ExtrudeEnd1()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ExtrudeSketch¶
-
BendInsertDesignBuilder.
ExtrudeSketch
¶ Returns the extrude sketch.
-------------------------------------
Getter Method
Signature
ExtrudeSketch()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
ExtrudeStart¶
-
BendInsertDesignBuilder.
ExtrudeStart
¶ Returns the extrude start, A half when composite insert.
-------------------------------------
Getter Method
Signature
ExtrudeStart()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ExtrudeStart1¶
-
BendInsertDesignBuilder.
ExtrudeStart1
¶ Returns the extrude start - B half.
-------------------------------------
Getter Method
Signature
ExtrudeStart1()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
FalseBody¶
-
BendInsertDesignBuilder.
FalseBody
¶ Returns or sets the false body creation option.
-------------------------------------
Getter Method
Signature
FalseBody()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FalseBody(falseBody)
Parameters: falseBody (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
FlipTrimDirection¶
-
BendInsertDesignBuilder.
FlipTrimDirection
¶ Returns or sets the flip trim feature direction of insert.
-------------------------------------
Getter Method
Signature
FlipTrimDirection()
Returns: Return type: bool New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipTrimDirection(flipTrimDirection)
Parameters: flipTrimDirection (bool) – New in version NX9.0.1.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
InsertComponent¶
-
BendInsertDesignBuilder.
InsertComponent
¶ Returns the select insert to delete
-------------------------------------
Getter Method
Signature
InsertComponent()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
InsertToEdit¶
-
BendInsertDesignBuilder.
InsertToEdit
¶ Returns the select insert to edit
-------------------------------------
Getter Method
Signature
InsertToEdit()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
InsertType¶
-
BendInsertDesignBuilder.
InsertType
¶ Returns or sets the insert type.
-------------------------------------
Getter Method
Signature
InsertType()
Returns: Return type: NXOpen.Tooling.BendInsertDesignBuilderInsertTypeOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertType(insertType)
Parameters: insertType ( NXOpen.Tooling.BendInsertDesignBuilderInsertTypeOption
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
IntersectPlane¶
-
BendInsertDesignBuilder.
IntersectPlane
¶ Returns or sets the intersect plane.
-------------------------------------
Getter Method
Signature
IntersectPlane()
Returns: Return type: NXOpen.Plane
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntersectPlane(intersectPlane)
Parameters: intersectPlane ( NXOpen.Plane
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
IsAutoDatum¶
-
BendInsertDesignBuilder.
IsAutoDatum
¶ Returns or sets the auto datum plane
-------------------------------------
Getter Method
Signature
IsAutoDatum()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAutoDatum(isInner)
Parameters: isInner (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
NewPartName¶
-
BendInsertDesignBuilder.
NewPartName
¶ Returns or sets the new component name.
-------------------------------------
Getter Method
Signature
NewPartName()
Returns: Retruns the new component name Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewPartName(newPartNames)
Parameters: newPartNames (str) – Specifies the new component name New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ParentNode¶
-
BendInsertDesignBuilder.
ParentNode
¶ Returns or sets the parent node.
-------------------------------------
Getter Method
Signature
ParentNode()
Returns: Return type: NXOpen.Tooling.BendInsertDesignBuilderParentOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentNode(parentNode)
Parameters: parentNode ( NXOpen.Tooling.BendInsertDesignBuilderParentOption
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ParentPartName¶
-
BendInsertDesignBuilder.
ParentPartName
¶ Returns or sets the parent part name to create insert.
-------------------------------------
Getter Method
Signature
ParentPartName()
Returns: Retruns parent part name Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPartName(parentPart)
Parameters: parentPart (str) – Specifies the parent part name New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
PunchPlateClearance¶
-
BendInsertDesignBuilder.
PunchPlateClearance
¶ Returns or sets the clearance value of punch plate.
-------------------------------------
Getter Method
Signature
PunchPlateClearance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchPlateClearance(punchPlateClr)
Parameters: punchPlateClr (float) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ReName¶
-
BendInsertDesignBuilder.
ReName
¶ Returns or sets the rename option.
-------------------------------------
Getter Method
Signature
ReName()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReName(reName)
Parameters: reName (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
StripperPlateClearance¶
-
BendInsertDesignBuilder.
StripperPlateClearance
¶ Returns or sets the clearance value of stripper plate.
-------------------------------------
Getter Method
Signature
StripperPlateClearance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StripperPlateClearance(stripperPlateClr)
Parameters: stripperPlateClr (float) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Type¶
-
BendInsertDesignBuilder.
Type
¶ Returns or sets the operation type of bending insert design.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.BendInsertDesignBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.BendInsertDesignBuilderTypes
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
UseBottomPlateClearance¶
-
BendInsertDesignBuilder.
UseBottomPlateClearance
¶ Returns or sets the option to use bottom backing plate clearance.
-------------------------------------
Getter Method
Signature
UseBottomPlateClearance()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseBottomPlateClearance(useBPClearance)
Parameters: useBPClearance (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
UseDiePlateClearance¶
-
BendInsertDesignBuilder.
UseDiePlateClearance
¶ Returns or sets the option to use die plate clearance.
-------------------------------------
Getter Method
Signature
UseDiePlateClearance()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseDiePlateClearance(useDPClearance)
Parameters: useDPClearance (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
UsePunchPlateClearance¶
-
BendInsertDesignBuilder.
UsePunchPlateClearance
¶ Returns or sets the option to use punch plate clearance.
-------------------------------------
Getter Method
Signature
UsePunchPlateClearance()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsePunchPlateClearance(usePPClearance)
Parameters: usePPClearance (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
UseStripperPlateClearance¶
-
BendInsertDesignBuilder.
UseStripperPlateClearance
¶ Returns or sets the option to use stripper plate clearance.
-------------------------------------
Getter Method
Signature
UseStripperPlateClearance()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseStripperPlateClearance(useSPClearance)
Parameters: useSPClearance (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
AddInsertComponent¶
-
BendInsertDesignBuilder.
AddInsertComponent
¶ Add the new bend insert component
Signature
AddInsertComponent()
New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SetFaces¶
-
BendInsertDesignBuilder.
SetFaces
¶ Sets the face occurrences into builder attribute.
Signature
SetFaces(faceOccs)
Parameters: faceOccs (list of NXOpen.Face
) – array of face occurrencesNew in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
BendInsertDesignBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.