SessionVisualizationShadeSeeThruStyleType Enumeration¶
NXOpen.Preferences.SessionVisualizationShade.SeeThruStyleType is an alias for NXOpen.Preferences.SessionVisualizationShadeSeeThruStyleType
-
class
NXOpen.Preferences.
SessionVisualizationShadeSeeThruStyleType
¶ Bases:
object
Determines how translucency is applied to less important shaded geometry when See-Thru is enabled.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.PartVisualizationEmphasisSeeThruStyleType
instead.Enum Members
Displays less important shaded geometry as a translucent shell with a specified color. “
“OriginalColorShell”, “Displays less important shaded geometry as a translucent shell, preserving original shaded geometry colors. “
“Layers”, “Displays less important shaded geometry as translucent layers with a specified color. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-