PartVisualizationEmphasisSeeThruStyleType Enumeration¶
NXOpen.Preferences.PartVisualizationEmphasis.SeeThruStyleType is an alias for NXOpen.Preferences.PartVisualizationEmphasisSeeThruStyleType
-
class
NXOpen.Preferences.
PartVisualizationEmphasisSeeThruStyleType
¶ Bases:
object
Determines how translucency and color are used to de-emphasize shaded geometry.
Enum Members
Displays de-emphasized shaded geometry as a translucent shell with a single color. “
“OriginalColorShell”, “Displays de-emphasized shaded geometry as a translucent shell, preserving original colors. “
“Layers”, “Displays de-emphasized shaded geometry as translucent layers with a single color. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-