PartVisualizationNamesBorders Class¶
-
class
NXOpen.Preferences.
PartVisualizationNamesBorders
¶ Bases:
object
Represents the set of visualization preferences of entire Working Part coming under Names/borders Tab
To obtain an instance of this class, refer to
NXOpen.Preferences.PartPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
CharacterSize | Returns or sets the character size. |
ObjectNameDisplay | Returns or sets the object name display |
ShowModelViewBorders | Returns or sets the show model view border flag. |
ShowModelViewNames | Returns or sets the show model view names flag. |
Methods¶
Enumerations¶
PartVisualizationNamesBordersNameDisplay Enumeration | Describes the available options for object name display selection |
Property Detail¶
CharacterSize¶
-
PartVisualizationNamesBorders.
CharacterSize
¶ Returns or sets the character size.
Allows to define the size of the text in the object names
-------------------------------------
Getter Method
Signature
CharacterSize()
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CharacterSize(characterSize)
Parameters: characterSize (float) – New in version NX3.0.0.
License requirements: None.
ObjectNameDisplay¶
-
PartVisualizationNamesBorders.
ObjectNameDisplay
¶ Returns or sets the object name display
-------------------------------------
Getter Method
Signature
ObjectNameDisplay()
Returns: Return type: NXOpen.Preferences.PartVisualizationNamesBordersNameDisplay
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectNameDisplay(objectNameDisplay)
Parameters: objectNameDisplay ( NXOpen.Preferences.PartVisualizationNamesBordersNameDisplay
) –New in version NX3.0.0.
License requirements: None.
ShowModelViewBorders¶
-
PartVisualizationNamesBorders.
ShowModelViewBorders
¶ Returns or sets the show model view border flag.
allows to turn on and off the display of view borders.
-------------------------------------
Getter Method
Signature
ShowModelViewBorders()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowModelViewBorders(showModelViewBorders)
Parameters: showModelViewBorders (bool) – New in version NX3.0.0.
License requirements: None.
ShowModelViewNames¶
-
PartVisualizationNamesBorders.
ShowModelViewNames
¶ Returns or sets the show model view names flag.
Allows to turn on and off the display of view names.
-------------------------------------
Getter Method
Signature
ShowModelViewNames()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowModelViewNames(showModelViewNames)
Parameters: showModelViewNames (bool) – New in version NX3.0.0.
License requirements: None.