PartVisualizationNamesBordersNameDisplay Enumeration¶
NXOpen.Preferences.PartVisualizationNamesBorders.NameDisplay is an alias for NXOpen.Preferences.PartVisualizationNamesBordersNameDisplay
-
class
NXOpen.Preferences.
PartVisualizationNamesBordersNameDisplay
¶ Bases:
object
Describes the available options for object name display selection
Enum Members
each name in the work view current at the time of name creation “
“WorkView”, ” Work View places all namesin the current work view, even if the existing names had been defined in different views “
“AllViews”, ” All Views places all namesin the all views except the drawing member views”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-