PackagingMeasureBuilder Class¶
-
class
NXOpen.Motion.
PackagingMeasureBuilder
¶ Bases:
NXOpen.Motion.PackagingBuilder
This is the builder class to create or edit a Measure object.
To create a new instance of this class, use
NXOpen.Motion.PackagingCollection.CreateMeasureBuilder
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Condition | Returns or sets the measure condition defined at NXOpen.Motion.PackagingMeasureBuilderMeasureCondition |
Enable | Returns or sets the enable flag of NXOpen.Motion.Packaging object. |
MsType | Returns or sets the Measure type defined at NXOpen.Motion.PackagingMeasureBuilderMeasureType |
Name | Returns or sets the name of NXOpen.Motion.Packaging object. |
StopOnEvent | Returns or sets the Stop_On_Event flag of NXOpen.Motion.PackagingMeasure object |
Tag | Returns the Tag for this object. |
Threshold | Returns or sets the Measure threshold value |
ThresholdAngleExpression | Returns the Measure angular threshold expression value |
ThresholdExpression | Returns the Measure threshold expression value |
Tolerance | Returns or sets the Measure tolerance value |
ToleranceAngleExpression | Returns the Measure angular tolerance expression value |
ToleranceExpression | Returns the Measure tolerance expression value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetList1 | Returns geometry list 1 of NXOpen.Motion.Packaging object. |
GetList2 | Returns the geometry list 2 of NXOpen.Motion.PackagingMeasure object. |
GetObject | Returns the object currently being edited by this builder. |
GetSourceList | Gets the source geometry data. |
GetTargetList | Gets the target geometry data. |
SetList1 | Sets geometry list 1. |
SetList2 | Sets the geometry list 2. |
SetSourceList | Sets the source geometry data. |
SetTargetList | Sets the target geometry data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PackagingMeasureBuilderMeasureCondition Enumeration | Measure condition |
PackagingMeasureBuilderMeasureType Enumeration | Measure type |
Structs¶
PackagingMeasureBuilderGeometryData_Struct Struct | Represents geometry data. |
Property Detail¶
Condition¶
-
PackagingMeasureBuilder.
Condition
¶ Returns or sets the measure condition defined at
NXOpen.Motion.PackagingMeasureBuilderMeasureCondition
-------------------------------------
Getter Method
Signature
Condition()
Returns: Return type: NXOpen.Motion.PackagingMeasureBuilderMeasureCondition
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Condition(condition)
Parameters: condition ( NXOpen.Motion.PackagingMeasureBuilderMeasureCondition
) –New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
MsType¶
-
PackagingMeasureBuilder.
MsType
¶ Returns or sets the Measure type defined at
NXOpen.Motion.PackagingMeasureBuilderMeasureType
-------------------------------------
Getter Method
Signature
MsType()
Returns: Return type: NXOpen.Motion.PackagingMeasureBuilderMeasureType
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
MsType(mType)
Parameters: mType ( NXOpen.Motion.PackagingMeasureBuilderMeasureType
) –New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
StopOnEvent¶
-
PackagingMeasureBuilder.
StopOnEvent
¶ Returns or sets the Stop_On_Event flag of
NXOpen.Motion.PackagingMeasure
object-------------------------------------
Getter Method
Signature
StopOnEvent()
Returns: Return type: bool New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
StopOnEvent(stopOnEvent)
Parameters: stopOnEvent (bool) – New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
Threshold¶
-
PackagingMeasureBuilder.
Threshold
¶ Returns or sets the Measure threshold value
-------------------------------------
Getter Method
Signature
Threshold()
Returns: Return type: float New in version NX4.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.PackagingMeasureBuilder.ThresholdExpression
orNXOpen.Motion.PackagingMeasureBuilder.ThresholdAngleExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Threshold(threshold)
Parameters: threshold (float) – New in version NX4.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.PackagingMeasureBuilder.ThresholdExpression
orNXOpen.Motion.PackagingMeasureBuilder.ThresholdAngleExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
ThresholdAngleExpression¶
-
PackagingMeasureBuilder.
ThresholdAngleExpression
¶ Returns the Measure angular threshold expression value
-------------------------------------
Getter Method
Signature
ThresholdAngleExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
ThresholdExpression¶
-
PackagingMeasureBuilder.
ThresholdExpression
¶ Returns the Measure threshold expression value
-------------------------------------
Getter Method
Signature
ThresholdExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
Tolerance¶
-
PackagingMeasureBuilder.
Tolerance
¶ Returns or sets the Measure tolerance value
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX4.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.PackagingMeasureBuilder.ToleranceExpression
orNXOpen.Motion.PackagingMeasureBuilder.ToleranceAngleExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX4.0.0.
Deprecated since version NX8.0.0: Obtain the expression using
NXOpen.Motion.PackagingMeasureBuilder.ToleranceExpression
orNXOpen.Motion.PackagingMeasureBuilder.ToleranceAngleExpression
to query or edit it.License requirements: mechanisms (“MECHANISMS”)
ToleranceAngleExpression¶
-
PackagingMeasureBuilder.
ToleranceAngleExpression
¶ Returns the Measure angular tolerance expression value
-------------------------------------
Getter Method
Signature
ToleranceAngleExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
ToleranceExpression¶
-
PackagingMeasureBuilder.
ToleranceExpression
¶ Returns the Measure tolerance expression value
-------------------------------------
Getter Method
Signature
ToleranceExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
GetList2¶
-
PackagingMeasureBuilder.
GetList2
¶ Returns the geometry list 2 of
NXOpen.Motion.PackagingMeasure
object.Measure can have one or two lists defined. If the user defines two lists, then measurements will be done between each object in list 1 against each object in list 2.
Signature
GetList2()
Returns: Return type: list of NXOpen.DisplayableObject
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetSourceList¶
-
PackagingMeasureBuilder.
GetSourceList
¶ Gets the source geometry data.
Signature
GetSourceList()
Returns: Source geometry data Return type: list of NXOpen.Motion.PackagingMeasureBuilderGeometryData_Struct
New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
GetTargetList¶
-
PackagingMeasureBuilder.
GetTargetList
¶ Gets the target geometry data.
Signature
GetTargetList()
Returns: Target geometry data Return type: list of NXOpen.Motion.PackagingMeasureBuilderGeometryData_Struct
New in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
SetList2¶
-
PackagingMeasureBuilder.
SetList2
¶ Sets the geometry list 2.
Signature
SetList2(list2)
Parameters: list2 (list of NXOpen.DisplayableObject
) –New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
SetSourceList¶
-
PackagingMeasureBuilder.
SetSourceList
¶ Sets the source geometry data.
Signature
SetSourceList(sourceGeometryData)
Parameters: sourceGeometryData (list of NXOpen.Motion.PackagingMeasureBuilderGeometryData_Struct
) – Source geometry dataNew in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
SetTargetList¶
-
PackagingMeasureBuilder.
SetTargetList
¶ Sets the target geometry data.
Signature
SetTargetList(targetGeometryData)
Parameters: targetGeometryData (list of NXOpen.Motion.PackagingMeasureBuilderGeometryData_Struct
) – Target geometry dataNew in version NX7.5.0.
License requirements: mechanisms (“MECHANISMS”)
Validate¶
-
PackagingMeasureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.