ModelingViewOtherSectionAttrT_Struct Struct¶
NXOpen.ModelingView.OtherSectionAttrT is an alias for NXOpen.ModelingViewOtherSectionAttrT_Struct
-
class
NXOpen.
ModelingViewOtherSectionAttrT_Struct
¶ Bases:
object
This defines the attributes data for dynamic sectioning
Deprecated since version NX5.0.0: This funcitonality is replaced by
NXOpen.ModelingView.ActiveDynamicSection
Fields¶
Field | Description |
---|---|
Lock | If true, all enabled planes are moved as a group |
CapType | Enable or disable capping |
CapColor | capping color index from UG’s color table |
TotalPlanesActive | Either 1/2/6 planes can be active at a time |
ActivePlane | To select the ‘active’ plane (of the 2 set) |
Lock¶
-
ModelingViewOtherSectionAttrT_Struct.
Lock
¶ If true, all enabled planes are moved as a group
-------------------------------------
Getter Method Signature
Lock()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
Lock(value)
Parameters: value (bool) –
CapType¶
-
ModelingViewOtherSectionAttrT_Struct.
CapType
¶ Enable or disable capping
-------------------------------------
Getter Method Signature
CapType()
Returns: Return type: NXOpen.ModelingViewSectionCap
-------------------------------------
Setter Method
Signature
CapType(value)
Parameters: value ( NXOpen.ModelingViewSectionCap
) –
CapColor¶
-
ModelingViewOtherSectionAttrT_Struct.
CapColor
¶ capping color index from UG’s color table
-------------------------------------
Getter Method Signature
CapColor()
Returns: Return type: int -------------------------------------
Setter Method
Signature
CapColor(value)
Parameters: value (int) –
TotalPlanesActive¶
-
ModelingViewOtherSectionAttrT_Struct.
TotalPlanesActive
¶ Either 1/2/6 planes can be active at a time
-------------------------------------
Getter Method Signature
TotalPlanesActive()
Returns: Return type: int -------------------------------------
Setter Method
Signature
TotalPlanesActive(value)
Parameters: value (int) –
ActivePlane¶
-
ModelingViewOtherSectionAttrT_Struct.
ActivePlane
¶ To select the ‘active’ plane (of the 2 set)
-------------------------------------
Getter Method Signature
ActivePlane()
Returns: Return type: NXOpen.ModelingViewSectionPlane
-------------------------------------
Setter Method
Signature
ActivePlane(value)
Parameters: value ( NXOpen.ModelingViewSectionPlane
) –