ModelingViewSectionCap Enumeration¶
NXOpen.ModelingView.SectionCap is an alias for NXOpen.ModelingViewSectionCap
-
class
NXOpen.
ModelingViewSectionCap
¶ Bases:
object
Defines whether to disable and enable capping.
If enabled, the capping color can be further defined by ‘cap_color’, or using the color of the solid that is being sectioned. If desired, solid interference check can also be enabled for visual inspection .. deprecated:: NX5.0.0
This funcitonality is replaced byNXOpen.ModelingView.ActiveDynamicSection
Enum Members
Enum Member Enum Member Description Off disableOn enable using cap_colorBodyColor enable using color of solid bodyBodyColorAndInterference with interference check-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-