ElectricalPartBuilder Class¶
-
class
NXOpen.Mechatronics.
ElectricalPartBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ElectricalPart
builderTo create a new instance of this class, use
NXOpen.Mechatronics.ElectricalPartCollection.CreateElectricalPartBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
PartNumber | Returns or sets the part number |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAttributes | Get the attributes data. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOwner | Get the owner system object. |
SetAttributes | Set the attributes data. |
SetOwner | Set the owner system object. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Structs¶
ElectricalPartBuilderAttribute_Struct Struct | Defined Attribute Structure |
Property Detail¶
PartNumber¶
-
ElectricalPartBuilder.
PartNumber
¶ Returns or sets the part number
-------------------------------------
Getter Method
Signature
PartNumber()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartNumber(partNumber)
Parameters: partNumber (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetAttributes¶
-
ElectricalPartBuilder.
GetAttributes
¶ Get the attributes data.
Signature
GetAttributes()
Returns: attribute array Return type: list of NXOpen.Mechatronics.ElectricalPartBuilderAttribute_Struct
New in version NX9.0.0.
License requirements: None.
GetOwner¶
-
ElectricalPartBuilder.
GetOwner
¶ Get the owner system object.
Signature
GetOwner()
Returns: Return type: NXOpen.Mechatronics.SystemObject
New in version NX9.0.0.
License requirements: None.
SetAttributes¶
-
ElectricalPartBuilder.
SetAttributes
¶ Set the attributes data.
Signature
SetAttributes(attribute)
Parameters: attribute (list of NXOpen.Mechatronics.ElectricalPartBuilderAttribute_Struct
) – attribute arrayNew in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetOwner¶
-
ElectricalPartBuilder.
SetOwner
¶ Set the owner system object.
Signature
SetOwner(owner)
Parameters: owner ( NXOpen.Mechatronics.SystemObject
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ElectricalPartBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.