SystemObject Class¶
-
class
NXOpen.Mechatronics.
SystemObject
¶ Bases:
NXOpen.NXObject
Represents the System Object.
System Object is the entity displaying in System Navigator. This is an abstract class and cannot be created.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddComponent | Adds Assemblies.Component . |
AddOperation | Adds operation object. |
AddPhysicsObjects | Adds behavioral physics objects. |
AddSignalAdapters | Adds signal adapter objects. |
ApplyNamingRule | Perform naming rule check and update the designation. |
AssociateItem | Associate a specified item to this system object. |
CreateTraceLink | Creates the trace link for system objects. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
DissociateItem | Dissociate a specified item from this system object. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAssociateItem | Query the associated item with a specified type. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetPhysicsObjects | Gets behavioral physics objects. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSingleDesignation | Get the single designation including aspect, letter code and index. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
RemoveComponent | Removes Assemblies.Component . |
RemoveOperation | Removes operation object. |
RemovePhysicsObjects | Removes behavioral physics objects. |
RemoveSignalAdapters | Removes signal adapter objects. |
RemoveTraceLink | Removes the trace link for system objects. |
RenameInstance | Renames system object instance. |
ReorderObject | Reorders system objects. |
RestructureObject | Restructure system object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSingleDesignation | Set the single designation including aspect, letter code and index. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
SystemObjectRelationType Enumeration | Relation type. |
SystemObjectReorderType Enumeration | Reorder object type to specify the relative position. |
Property Detail¶
IsOccurrence¶
-
SystemObject.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SystemObject.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SystemObject.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SystemObject.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SystemObject.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SystemObject.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddComponent¶
-
SystemObject.
AddComponent
¶ Adds
Assemblies.Component
.Signature
AddComponent(comps)
Parameters: comps (list of NXOpen.Assemblies.Component
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AddOperation¶
-
SystemObject.
AddOperation
¶ Adds operation object.
Signature
AddOperation(opers)
Parameters: opers (list of NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AddPhysicsObjects¶
-
SystemObject.
AddPhysicsObjects
¶ Adds behavioral physics objects.
Signature
AddPhysicsObjects(objects)
Parameters: objects (list of NXOpen.NXObject
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AddSignalAdapters¶
-
SystemObject.
AddSignalAdapters
¶ Adds signal adapter objects.
Signature
AddSignalAdapters(adapters)
Parameters: adapters (list of NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ApplyNamingRule¶
-
SystemObject.
ApplyNamingRule
¶ Perform naming rule check and update the designation.
Signature
ApplyNamingRule()
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AssociateItem¶
-
SystemObject.
AssociateItem
¶ Associate a specified item to this system object.
This method only makes sense in NX Manager mode.
Signature
AssociateItem(type, itemMFKID, revisionID)
Parameters: - type (
NXOpen.Mechatronics.SystemObjectRelationType
) – The relation type. - itemMFKID (str) – The item MFK ID of association item.
- revisionID (str) – The revision ID of association item.
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
- type (
CreateTraceLink¶
-
SystemObject.
CreateTraceLink
¶ Creates the trace link for system objects.
This method only makes sense in NX Manager mode.
Signature
CreateTraceLink(pComplying)
Parameters: pComplying ( NXOpen.Mechatronics.SystemObject
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DissociateItem¶
-
SystemObject.
DissociateItem
¶ Dissociate a specified item from this system object.
This method only makes sense in NX Manager mode.
Signature
DissociateItem(itemMFKID, revisionID)
Parameters: - itemMFKID (str) – The item MFK ID of dissociation item.
- revisionID (str) – The revision ID of dissociation item.
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
SystemObject.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAssociateItem¶
-
SystemObject.
GetAssociateItem
¶ Query the associated item with a specified type.
This method only makes sense in NX Manager mode.
Signature
GetAssociateItem(type)
Parameters: type ( NXOpen.Mechatronics.SystemObjectRelationType
) – The relation type.Returns: a tuple Return type: A tuple consisting of (itemMFKID, revisionID). itemMFKID is a str. The item MFK ID of association item. revisionID is a str. The revision ID of association item. New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetPhysicsObjects¶
-
SystemObject.
GetPhysicsObjects
¶ Gets behavioral physics objects.
Signature
GetPhysicsObjects()
Returns: Return type: list of NXOpen.NXObject
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetSingleDesignation¶
-
SystemObject.
GetSingleDesignation
¶ Get the single designation including aspect, letter code and index.
Signature
GetSingleDesignation()
Returns: Return type: str New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Print¶
-
SystemObject.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveComponent¶
-
SystemObject.
RemoveComponent
¶ Removes
Assemblies.Component
.Signature
RemoveComponent(comps)
Parameters: comps (list of NXOpen.Assemblies.Component
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RemoveOperation¶
-
SystemObject.
RemoveOperation
¶ Removes operation object.
Signature
RemoveOperation(opers)
Parameters: opers (list of NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RemovePhysicsObjects¶
-
SystemObject.
RemovePhysicsObjects
¶ Removes behavioral physics objects.
Signature
RemovePhysicsObjects(objects)
Parameters: objects (list of NXOpen.NXObject
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RemoveSignalAdapters¶
-
SystemObject.
RemoveSignalAdapters
¶ Removes signal adapter objects.
Signature
RemoveSignalAdapters(adapters)
Parameters: adapters (list of NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RemoveTraceLink¶
-
SystemObject.
RemoveTraceLink
¶ Removes the trace link for system objects.
This method only makes sense in NX Manager mode.
Signature
RemoveTraceLink(pComplying)
Parameters: pComplying ( NXOpen.Mechatronics.SystemObject
) –New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RenameInstance¶
-
SystemObject.
RenameInstance
¶ Renames system object instance.
Signature
RenameInstance(name)
Parameters: name (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ReorderObject¶
-
SystemObject.
ReorderObject
¶ Reorders system objects.
The method will reorder the objects in the same level of the structure. The source object will be moved to the destination and the sibling will update the order accordingly.
Signature
ReorderObject(pDestination, beforeOrAfter)
Parameters: - pDestination (
NXOpen.Mechatronics.SystemObject
) – - beforeOrAfter (
NXOpen.Mechatronics.SystemObjectReorderType
) – Reorder Before/After
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
- pDestination (
RestructureObject¶
-
SystemObject.
RestructureObject
¶ Restructure system object.
Signature
RestructureObject(pDestination)
Parameters: pDestination ( NXOpen.Mechatronics.SystemObject
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetName¶
-
SystemObject.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSingleDesignation¶
-
SystemObject.
SetSingleDesignation
¶ Set the single designation including aspect, letter code and index.
The aspect, letter code and index are joined together and comply with the rules defined in the configuration file.
Signature
SetSingleDesignation(designation)
Parameters: designation (str) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)